SilhouetteMatch

This tutorial shows how to use the SilhouetteMatch module with Basler’s partner Roboception’s URCap.

Before we start

This tutorial assumes that you are familiar with the Generic rc_visard node and that a valid hand-eye calibration has been stored on the rc_visard as described in Hand-Eye Calibration.

Overview

The SilhouetteMatch functionality is available in the generic rc_visard node. Please see Generic rc_visard node in order to learn how to work with generic rc_visard nodes.

The following functions are available for SilhouetteMatch:

  • Detect: Triggers detection
  • GetObjectPose: Gets the next object pose after detection has been triggered
  • GetNextGrasp: Gets the next grasp after detection has been triggered
  • GetLCPose: Gets the pose of the detected load carrier
  • CalibratePlane: Starts the base plane calibration
  • SetPreferredOrientation: Sets the Preferred Orientation based on the stored robot pose

Detect

../_images/sil_detect.png

It is mandatory to choose the template that has to be detected. If necessary, enter a region of interest, load carrier, gripper and offset.

GetObjectPose

../_images/sil_get_object_pose.png

This function requires that the Detect function has been triggered before. It returns the pose of the next available object that was detected and stores the pose in PolyScope’s variable format.

If no reachable template is matched and the Stop program when pose is not available checkbox is checked, a popup will appear and the program will be terminated. If the checkbox is not checked, a zero pose (p[0,0,0,0,0,0]) will be returned.

Note

When the Stop program when pose is not available checkbox is unchecked, the user has to catch the case when nothing is detected (the zero pose (p[0,0,0,0,0,0]) is returned). If this situation is not handled, it might lead to collision or undefined robot behavior.

With the ‘Pick approach angle’ drop-down menu it is possible to change the strategy of calculating the angle of the returned pose. There are four different options to choose from:

  • Last waypoint orientation The detected orientation is ignored, instead the orientation of the last waypoint is used.
  • Only RZ from detected pose For RZ the detected orientation is used, RX and RY are based on the last waypoint orientation.
  • Only RX, RY from detected pose For RX and RY the detected orientation is used, RZ is based on the last waypoint orientation.
  • Detected pose orientation The complete detected orientation is used.

GetNextGrasp

../_images/sil_get_next_grasp.png

This functions requires that Detect has been triggered before. It assigns the next available grasp pose and stores the pose in PolyScope’s variable format (p[x, y, z, rx, ry, rz]). It is also possible to store the grasp ID associated with this grasp.

If no reachable grasp is detected and the Stop program when pose is not available checkbox is checked, a popup will appear and the program will be terminated. If the checkbox is not checked, a zero pose (p[0,0,0,0,0,0]) will be returned.

Note

When the Stop program when pose is not available checkbox is unchecked, the user has to catch the case when nothing is detected (the zero pose (p[0,0,0,0,0,0]) is returned). If this situation is not handled, it might lead to collision or undefined robot behavior.

With the ‘Pose orientation’ drop down menu it is possible to change the strategy of calculating the angle of the returned position. There are four different options to choose from:

  • Last waypoint orientation Detected orientation is ignored, instead the orientation of the last waypoint is used.
  • Only RZ from detected pose For RZ detected orientation is used, RX and RY are based on the last waypoint orientation.
  • Only RX, RY from detected pose For RX RY detected orientation is used, RZ is based on the last waypoint orientation.
  • Detected pose orientation The complete detected orientation is used.

GetLcPose

../_images/sil_get_lc_pose.png

This function requires that Detect has been triggered with a load carrier ID. It returns the pose of the detected load carrier. If no load carrier is detected, a zero pose (p[0,0,0,0,0,0]) will be returned.

Note

When the Stop program when pose is not available checkbox is unchecked, the user has to catch the case when nothing is detected (the zero pose (p[0,0,0,0,0,0]) is returned). If this situation is not handled, it might lead to collision or undefined robot behavior.

CalibratePlane

../_images/sil_calibrate_plane.png

This function starts the base plane calibration procedure.

SetPreferredOrientation

../_images/sil_set_preferred_orientation.png

This function sets the Preferred Orientation based on the stored robot pose. If it is not required to change this value during program execution, this node should be put in the Before Start section.