Safety

Warning

The operator must have read and understood all of the instructions in this manual before handling the rc_cube product.

Warning

If operating the rc_cube with rc_visard product(s), the operator must have read and understood all of the safety, installation, and maintenance instructions given in the rc_visard manual.

Note

The term “operator” refers to anyone responsible for any of the following tasks performed in conjunction with rc_cube:

  • Installation
  • Maintenance
  • Inspection
  • Calibration
  • Programming
  • Decommissioning

This manual explains the rc_cube’s various components and general operations regarding the product’s whole life-cycle, from installation through operation to decommissioning.

The drawings and photos in this documentation are representative examples; differences may exist between them and the delivered product.

General warnings

Note

Any use of the rc_cube in noncompliance with these warnings is inappropriate and may cause injury or damage as well as void the warranty.

Warning

  • The rc_cube’s and any related equipment’s safety guidelines must always be satisfied.
  • The rc_cube does not fall under the purview of the machinery or medical directives.

Intended use

The rc_cube is intended to be used in combination with a 3D camera for data acquisition (e.g., stereo images). It is furthermore intended to process that data using 3D-image processing algorithms to serve in applications such as object detection or robotic pick-and-place.

Warning

The rc_cube is only intended for stationary installation.

Warning

The rc_cube is NOT intended for safety critical applications.

The GigE Vision® industry standard used by the rc_cube does not support authentication and encryption. All data from and to the device is transmitted without authentication and encryption and could be monitored or manipulated by a third party. It is the operator’s responsibility to connect the rc_cube only to a secured internal network.

Warning

The rc_cube must be connected to secured internal networks.

The rc_cube may be used only within the scope of its technical specification. Any other use of the product is deemed unintended use. Basler will not be liable for any damages resulting from any improper or unintended use.

Warning

Always comply with local and/or national laws, regulations and directives on automation safety and general machine safety.