Auto Function ROI#
ROI is short for region of interest (formerly AOI = area of interest).
You can create several auto function ROIs, each occupying different parts of the sensor array.
The settings for the Auto Function ROI feature are independent of the settings for the Image ROI feature.
Using the Feature#
Changing Position and Size of an Auto Function ROI#
By default, all auto function ROIs are set to the same size as the camera's image ROI. You can change their positions and sizes to suit your needs.
To change the position and size of an auto function ROI:
- Set the
AutoFunctionROISelector
parameter to one of the available auto function ROIs, e.g.,ROI1
. -
Enter values for the following parameters to specify the position of the auto function ROI selected:
AutoFunctionROIOffsetX
AutoFunctionROIOffsetY
-
Enter values for the following parameters to specify the size of the auto function ROI selected:
AutoFunctionROIWidth
AutoFunctionROIHeight
The position of an auto function ROI is specified based on the lines and rows of the sensor array.
Example: Assume that you have selected auto function ROI 1 and specified the following settings:
AutoFunctionROIOffsetX
= 14AutoFunctionROIOffsetY
= 7AutoFunctionROIWidth
= 5AutoFunctionROIHeight
= 6
This creates the following auto function ROI 1:
Only the pixel data from the area of overlap between the auto function ROI and the image ROI will be used by the auto function assigned to it.
Info
- On color cameras, Basler recommends setting the parameters for position and size to even values (multiples of 2). This matches the auto function ROI to the color filter pattern of the sensor.
- On racer 2 S cameras with CXP interface, the
AutoFunctionROIHeight
parameter is automatically set to 0 and can't be changed. - On racer 2 S cameras with GigE or 5GigE interface where you can work with frames containing more than one line, you can set the
AutoFunctionROIHeight
parameter to a value bigger than 1. - If the Binning feature is enabled, the auto function ROI settings refer to the binned lines and columns and not to the physical lines in the sensor.
- If the Reverse X or Reverse Y feature or both are enabled, the position of the auto function ROI relative to the sensor remains the same. As a consequence, different regions of the image will be controlled depending on whether or not Reverse X, Reverse Y or both are enabled.
Auto Function ROI Highlighting#
If highlighting is supported by your camera model, you can highlight one or multiple Auto Function ROIs in the pylon Viewer. Areas that don't belong to the Auto Function ROIs appear darker:
To highlight an Auto Function ROI:
- Set the
AutoFunctionROISelector
parameter to the desired auto function ROI, e.g.,ROI1
. - Set the
AutoFunctionROIHighlight
parameter totrue
.
Assigning Auto Functions#
By default, each auto function ROI is assigned to a specific auto function. For example, the pixel data from auto function ROI 2 is used to control the Balance White Auto auto function.
On some camera models, the default assignments can be changed. To do so:
Set the AutoFunctionROISelector
parameter to one of the available auto function ROIs, e.g., ROI1
.
Assign the desired auto functions to the auto function ROI selected:
- If you want to assign Balance White Auto, set the
AutoFunctionROIUseWhiteBalance
parameter totrue
. - If you want to assign Exposure Auto and Gain Auto, set the
AutoFunctionROIUseBrightness
parameter totrue
. (Exposure Auto and Gain Auto always work together.) - If you want to assign Tonal Range Auto, set the
AutoFunctionROIUseTonalRange
parameter totrue
.
Info
- If you assign one auto function to multiple auto function ROIs, the pixel data from all selected auto function ROIs will be used for the auto function.
- If you assign multiple auto functions to one auto function ROI, the pixel data from the auto function ROI will be used for all auto functions selected.
Exposure Auto and Gain Auto Assignments Work Together#
When making auto function ROI assignments, the Gain Auto auto function and the exposure auto auto function always work together. They are considered as a single auto function named "intensity" or "brightness", depending on your camera model.
This does not imply, however, that Gain Auto and Exposure Auto must always be enabled at the same time.
Guidelines#
When you are setting an auto function ROI, you must follow these guidelines:
Guideline | Example |
---|---|
AutoFunctionROIOffsetX + AutoFunctionROIWidth ≤ Width of camera sensor | Camera with a 1920 x 1080 pixel sensor:AutoFunctionROIOffsetX + AutoFunctionROIWidth ≤ 1920 |
AutoFunctionROIOffsetY + AutoFunctionROIHeight ≤ Height of camera sensor | Camera with a 1920 x 1080 pixel sensor:AutoFunctionROIOffsetY + AutoFunctionROIHeight ≤ 1080 |
Overlap Between Auto Function ROI and Image ROI#
The size and position of an auto function ROI can be identical to the size and position of the image ROI, but this is not a requirement. For an auto function to work, it is sufficient if both ROIs overlap each other partially.
The overlap between auto function ROI and image ROI determines whether and to what extent the auto function will control the related image property. Only the pixel data from the areas of overlap will be used by the auto function to control the image property of the entire image.
-
If the auto function ROI is completely contained in the image ROI, the pixel data from the auto function ROI will be used to control the image property.
-
If the image ROI is completely contained in the auto function ROI, only the pixel data from the image ROI will be used to control the image property.
-
If the auto function ROI overlaps the image ROI only partially, only the pixel data from the area of partial overlap will be used to control the image property.
-
If the auto function ROI does not overlap the image ROI, the related auto function will not work.
Info
Basler strongly recommends completely including the auto function ROI within the image ROI or choosing identical positions and sizes for auto function ROI and image ROI.
Specifics#
Camera Model | Auto Function ROIs | Default Assignments | Assignments Can Be Changed | Highlighting Supported |
---|---|---|---|---|
a2A640-240gmSWIR | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A640-240umSWIR | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A1280-80gmSWIR | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A1280-125umSWIR | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A1920-51gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A1920-51gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A1920-51gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A1920-51gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A1920-160ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A1920-160ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A1920-160umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A1920-160umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A1920-165g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A1920-165g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2048-35gmSWIR | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2048-37gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2048-37gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2048-37gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2048-37gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2048-110umSWIR | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2048-114g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2048-114g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2048-114ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2048-114ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2048-114umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2048-114umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2440-98g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2440-98g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2448-23gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2448-23gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2448-23gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2448-23gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2448-75ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2448-75ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2448-75umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2448-75umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2448-105g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2448-105g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2448-120cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2448-120cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
a2A2448-210cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2448-210cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
a2A2560-20gmSWIR | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2560-70umSWIR | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2590-22gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2590-22gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2590-22gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2590-22gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2590-60ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2590-60ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2590-60umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2590-60umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2600-20gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2600-20gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2600-20gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2600-20gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2600-64ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2600-64ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2600-64umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2600-64umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2840-14gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2840-14gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2840-14gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2840-14gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2840-14gmUV | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2840-48ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2840-48ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2840-48umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2840-48umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2840-48umUV | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2840-67g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2840-67g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2840-67g5mUV | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A2840-86cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A2840-86cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
a2A3536-9gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A3536-9gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A3536-9gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A3536-9gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A3536-31ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A3536-31ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A3536-31umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A3536-31umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A3536-42g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A3536-42g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A3840-13gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A3840-13gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A3840-13gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A3840-13gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A3840-45ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A3840-45ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A3840-45umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A3840-45umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4096-9gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4096-9gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4096-9gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4096-9gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4096-30ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4096-30ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4096-30umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4096-30umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4096-44g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4096-44g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4096-67cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4096-67cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
a2A4200-12gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4200-12gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4200-12gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4200-12gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4200-40ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4200-40ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4200-40umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4200-40umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4504-5gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4504-5gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4504-5gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4504-5gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4504-18ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4504-18ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4504-18umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4504-18umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4504-27g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4504-27g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4504-42cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4504-42cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
a2A4508-6gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4508-6gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4508-6gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4508-6gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4508-20ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4508-20ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A4508-20umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A4508-20umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5060-4gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5060-4gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5060-15ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5060-15umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5060-21g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5060-21g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5060-35cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5060-35cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
a2A5320-7gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5320-7gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5320-7gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5320-7gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5320-23ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5320-23ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5320-23umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5320-23umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5320-34g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5320-34g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5320-52cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5320-52cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
a2A5328-4gcBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5328-4gcPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5328-4gmBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5328-4gmPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5328-15ucBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5328-15ucPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5328-15umBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5328-15umPRO | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5328-22g5cBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5328-22g5mBAS | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
a2A5328-35cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
a2A5328-35cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
acA640-121gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA640-300gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA640-300gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA640-750uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA640-750um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA720-290gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA720-290gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA720-520uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA720-520um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA800-200gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA800-200gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA800-510uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA800-510um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1280-60gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1280-60gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1300-60gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1300-60gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1300-60gmNIR | ROI 1 ROI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1300-75gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1300-75gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1300-200uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1300-200um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1440-73gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1440-73gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1440-220uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1440-220um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1600-20gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1600-20uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1600-60gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1600-60gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-25gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-25gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-25uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-25um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-40gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-40gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-40uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-40ucMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA1920-40um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-40umMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA1920-48gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-48gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-50gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-50gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-150uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-150um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-155uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-155ucMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA1920-155um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA1920-155umMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA2000-50gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2000-50gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2000-165uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2000-165um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-25gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-25gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-25gmNIR | ROI 1 ROI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-35gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-35gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-55uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-55um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-90uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-90um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-90umNIR | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-120uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2040-120um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2440-20gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2440-20gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2440-35uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2440-35ucMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA2440-35um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2440-35umMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA2440-75uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2440-75ucMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA2440-75um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2440-75umMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA2500-14gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2500-14gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2500-14uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2500-14um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2500-20gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2500-20gcMED | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA2500-20gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA2500-20gmMED | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA2500-60uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA2500-60um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA3088-16gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA3088-16gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA3088-57uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA3088-57ucMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA3088-57um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA3088-57umMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA3800-10gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA3800-10gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA3800-14uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA3800-14um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4024-8gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA4024-8gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA4024-29uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4024-29um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4096-11gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA4096-11gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA4096-30uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4096-30ucMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA4096-30um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4096-30umMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA4096-40uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4096-40ucMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA4096-40um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4096-40umMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA4112-8gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA4112-8gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA4112-20uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4112-20ucMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA4112-20um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4112-20umMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA4112-30uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4112-30ucMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA4112-30um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA4112-30umMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA5472-5gc | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA5472-5gm | AOI 1 AOI 2 | AOI 1: Intensity (Gain Auto + Exposure Auto) AOI 2: White Balance (Balance White Auto) | Yes | No |
acA5472-17uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA5472-17ucMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
acA5472-17um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | No |
acA5472-17umMED | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto), Tonal Range (Tonal Range Auto) | Yes | No |
boA1936-400cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA1936-400cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
boA2448-250cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA2448-250cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
boA2832-190cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA2832-190cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
boA4096-93cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA4096-93cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
boA4096-180cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA4096-180cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
boA4112-68cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA4112-68cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
boA4500-45cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA4500-45cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
boA4504-100cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA4504-100cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
boA5120-150cc | ROI 1 | ROI 1: White Balance (Balance White Auto) | No | Yes |
boA5120-150cm | ROI 1 | ROI 1: White Balance (Balance White Auto) | No | Yes |
boA5120-230cc | ROI 1 | ROI 1: White Balance (Balance White Auto) | No | Yes |
boA5120-230cm | ROI 1 | ROI 1: White Balance (Balance White Auto) | No | Yes |
boA5320-150cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA5320-150cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
boA5328-100cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA5328-100cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
boA6500-36cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA6500-36cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
boA8100-16cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
boA8100-16cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
boA9344-30cc | ROI 1 | ROI 1: White Balance (Balance White Auto) | No | Yes |
boA9344-30cm | ROI 1 | ROI 1: White Balance (Balance White Auto) | No | Yes |
boA9344-70cc | ROI 1 | ROI 1: White Balance (Balance White Auto) | No | Yes |
boA9344-70cm | ROI 1 | ROI 1: White Balance (Balance White Auto) | No | Yes |
boA13440-17cm | Auto Function ROI feature not supported | Auto Function ROI feature not supported | - | - |
daA720-520uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
daA720-520um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
daA1280-54uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
daA1280-54um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
daA1440-220uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
daA1440-220um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
daA1600-60uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
daA1600-60um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
daA1920-15um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
daA1920-30uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
daA1920-30um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
daA1920-160uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
daA1920-160um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
daA2448-70uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
daA2448-70um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
daA2500-14uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
daA2500-14um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
daA3840-45uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
daA3840-45um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Not assigned | Yes | Yes |
dmA720-290gc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
dmA720-290gm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
dmA1440-73gc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
dmA1440-73gm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
dmA1920-51gc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
dmA1920-51gm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
dmA2048-37gc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
dmA2048-37gm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
dmA2448-23gc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
dmA2448-23gm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
dmA2840-14gc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
dmA2840-14gm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
dmA3536-9gc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
dmA3536-9gm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
dmA4096-9gc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
dmA4096-9gm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: Brightness (Gain Auto + Exposure Auto) | Yes | Yes |
puA1280-54uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
puA1280-54um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
puA1600-60uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
puA1600-60um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
puA1920-30uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
puA1920-30um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
puA2500-14uc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
puA2500-14um | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | No | No |
r2L2048-29gc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
r2L2048-58gm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: - | Yes | Yes |
r2L2048-62cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
r2L2048-62g5c | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
r2L2048-172cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: - | Yes | Yes |
r2L2048-172g5m | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: - | Yes | Yes |
r2L4096-14gc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
r2L4096-29gm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: - | Yes | Yes |
r2L4096-42cc | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
r2L4096-42g5c | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: White Balance (Balance White Auto) | Yes | Yes |
r2L4096-84cm | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: - | Yes | Yes |
r2L4096-84g5m | ROI 1 ROI 2 | ROI 1: Brightness (Gain Auto + Exposure Auto) ROI 2: - | Yes | Yes |
r2L8192-200cm | Auto Function ROI feature not supported | Auto Function ROI feature not supported | - | - |
r2L16384-120cm | Auto Function ROI feature not supported | Auto Function ROI feature not supported | - | - |
Sample Code#
ace 2, boost, and dart R Cameras#
// Select auto function ROI 1
camera.AutoFunctionROISelector.SetValue(AutoFunctionROISelector_ROI1);
// Specify position and size of the auto function ROI selected
camera.AutoFunctionROIOffsetX.SetValue(10);
camera.AutoFunctionROIOffsetY.SetValue(10);
camera.AutoFunctionROIWidth.SetValue(500);
camera.AutoFunctionROIHeight.SetValue(400);
// Enable Balance White Auto for the auto function ROI selected
camera.AutoFunctionROIUseWhiteBalance.SetValue(true);
// Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
camera.AutoFunctionROIUseBrightness.SetValue(true);
// Highlight the auto function ROI selected
camera.AutoFunctionROIHighlight.SetValue(true);
INodeMap& nodemap = camera.GetNodeMap();
// Select auto function ROI 1
CEnumParameter(nodemap, "AutoFunctionROISelector").SetValue("ROI1");
// Specify position and size of the auto function ROI selected
CIntegerParameter(nodemap, "AutoFunctionROIOffsetX").SetValue(10);
CIntegerParameter(nodemap, "AutoFunctionROIOffsetY").SetValue(10);
CIntegerParameter(nodemap, "AutoFunctionROIWidth").SetValue(500);
CIntegerParameter(nodemap, "AutoFunctionROIHeight").SetValue(400);
// Enable Balance White Auto for the auto function ROI selected
CBooleanParameter(nodemap, "AutoFunctionROIUseWhiteBalance").SetValue(true);
// Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
CBooleanParameter(nodemap, "AutoFunctionROIUseBrightness").SetValue(true);
// Highlight the auto function ROI selected
CBooleanParameter(nodemap, "AutoFunctionROIHighlight").SetValue(true);
// Select auto function ROI 1
camera.Parameters[PLCamera.AutoFunctionROISelector].SetValue(PLCamera.AutoFunctionROISelector.ROI1);
// Specify position and size of the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionROIOffsetX].SetValue(10);
camera.Parameters[PLCamera.AutoFunctionROIOffsetY].SetValue(10);
camera.Parameters[PLCamera.AutoFunctionROIWidth].SetValue(500);
camera.Parameters[PLCamera.AutoFunctionROIHeight].SetValue(400);
// Enable Balance White Auto for the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionROIUseWhiteBalance].SetValue(true);
// Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionROIUseBrightness].SetValue(true);
// Highlight the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionROIHighlight].SetValue(true);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Select auto function ROI 1 */
errRes = PylonDeviceFeatureFromString(hdev, "AutoFunctionROISelector", "ROI1");
CHECK(errRes);
/* Specify position and size of the auto function ROI selected */
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionROIOffsetX", 10);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionROIOffsetY", 10);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionROIWidth", 500);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionROIHeight", 400);
CHECK(errRes);
/* Enable Balance White Auto for the auto function ROI selected */
errRes = PylonDeviceSetBooleanFeature(hdev, "AutoFunctionROIUseWhiteBalance", 1);
CHECK(errRes);
/* Enable the 'Brightness' auto function (Gain Auto + Exposure Auto) */
/* for the auto function ROI selected */
errRes = PylonDeviceSetBooleanFeature(hdev, "AutoFunctionROIUseBrightness", 1);
CHECK(errRes);
/* Highlight the auto function ROI selected */
errRes = PylonDeviceSetBooleanFeature(hdev, "AutoFunctionROIHighlight", 1);
CHECK(errRes);
# Select auto function ROI 1
camera.AutoFunctionROISelector.Value = "ROI1"
# Specify position and size of the auto function ROI selected
camera.AutoFunctionROIOffsetX.Value = 10
camera.AutoFunctionROIOffsetY.Value = 10
camera.AutoFunctionROIWidth.Value = 500
camera.AutoFunctionROIHeight.Value = 400
# Enable Balance White Auto for the auto function ROI selected
camera.AutoFunctionROIUseWhiteBalance.Value = True
# Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
# for the auto function ROI selected
camera.AutoFunctionROIUseBrightness.Value = True
# Highlight the auto function ROI selected
camera.AutoFunctionROIHighlight.Value = True
ace Classic/U/L GigE Cameras#
// Select auto function AOI 1
camera.AutoFunctionAOISelector.SetValue(AutoFunctionAOISelector_AOI1);
// Specify position and size of the auto function ROI selected
camera.AutoFunctionAOIOffsetX.SetValue(10);
camera.AutoFunctionAOIOffsetY.SetValue(10);
camera.AutoFunctionAOIWidth.SetValue(500);
camera.AutoFunctionAOIHeight.SetValue(400);
// Enable Balance White Auto for the auto function ROI selected
camera.AutoFunctionAOIUsageWhiteBalance.SetValue(true);
// Enable the 'Intensity' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
camera.AutoFunctionAOIUsageIntensity.SetValue(true);
INodeMap& nodemap = camera.GetNodeMap();
// Select auto function AOI 1
CEnumParameter(nodemap, "AutoFunctionAOISelector").SetValue("AOI1");
// Specify position and size of the auto function ROI selected
CIntegerParameter(nodemap, "AutoFunctionAOIOffsetX").SetValue(10);
CIntegerParameter(nodemap, "AutoFunctionAOIOffsetY").SetValue(10);
CIntegerParameter(nodemap, "AutoFunctionAOIWidth").SetValue(500);
CIntegerParameter(nodemap, "AutoFunctionAOIHeight").SetValue(400);
// Enable Balance White Auto for the auto function ROI selected
CBooleanParameter(nodemap, "AutoFunctionAOIUsageWhiteBalance").SetValue(true);
// Enable the 'Intensity' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
CBooleanParameter(nodemap, "AutoFunctionAOIUsageIntensity").SetValue(true);
// Select auto function AOI 1
camera.Parameters[PLCamera.AutoFunctionAOISelector].SetValue(PLCamera.AutoFunctionAOISelector.AOI1);
// Specify position and size of the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionAOIOffsetX].SetValue(10);
camera.Parameters[PLCamera.AutoFunctionAOIOffsetY].SetValue(10);
camera.Parameters[PLCamera.AutoFunctionAOIWidth].SetValue(500);
camera.Parameters[PLCamera.AutoFunctionAOIHeight].SetValue(400);
// Enable Balance White Auto for the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionAOIUsageWhiteBalance].SetValue(true);
// Enable the 'Intensity' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionAOIUsageIntensity].SetValue(true);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Select auto function AOI 1 */
errRes = PylonDeviceFeatureFromString(hdev, "AutoFunctionAOISelector", "AOI1");
CHECK(errRes);
/* Specify position and size of the auto function ROI selected */
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionAOIOffsetX", 10);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionAOIOffsetY", 10);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionAOIWidth", 500);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionAOIHeight", 400);
CHECK(errRes);
/* Enable Balance White Auto for the auto function ROI selected */
errRes = PylonDeviceSetBooleanFeature(hdev, "AutoFunctionAOIUsageWhiteBalance", 1);
CHECK(errRes);
/* Enable the 'Intensity' auto function (Gain Auto + Exposure Auto) */
/* for the auto function ROI selected */
errRes = PylonDeviceSetBooleanFeature(hdev, "AutoFunctionAOIUsageIntensity", 1);
CHECK(errRes);
# Select auto function AOI 1
camera.AutoFunctionAOISelector.Value = "AOI1"
# Specify position and size of the auto function ROI selected
camera.AutoFunctionAOIOffsetX.Value = 10
camera.AutoFunctionAOIOffsetY.Value = 10
camera.AutoFunctionAOIWidth.Value = 500
camera.AutoFunctionAOIHeight.Value = 400
# Enable Balance White Auto for the auto function ROI selected
camera.AutoFunctionAOIUsageWhiteBalance.Value = True
# Enable the 'Intensity' auto function (Gain Auto + Exposure Auto)
# for the auto function ROI selected
camera.AutoFunctionAOIUsageIntensity.Value = True
Other Cameras#
// Select auto function ROI 1
camera.AutoFunctionROISelector.SetValue(AutoFunctionROISelector_ROI1);
// Specify position and size of the auto function ROI selected
camera.AutoFunctionROIOffsetX.SetValue(10);
camera.AutoFunctionROIOffsetY.SetValue(10);
camera.AutoFunctionROIWidth.SetValue(500);
camera.AutoFunctionROIHeight.SetValue(400);
// Enable Balance White Auto for the auto function ROI selected
camera.AutoFunctionROIUseWhiteBalance.SetValue(true);
// Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
camera.AutoFunctionROIUseBrightness.SetValue(true);
INodeMap& nodemap = camera.GetNodeMap();
// Select auto function ROI 1
CEnumParameter(nodemap, "AutoFunctionROISelector").SetValue("ROI1");
// Specify position and size of the auto function ROI selected
CIntegerParameter(nodemap, "AutoFunctionROIOffsetX").SetValue(10);
CIntegerParameter(nodemap, "AutoFunctionROIOffsetY").SetValue(10);
CIntegerParameter(nodemap, "AutoFunctionROIWidth").SetValue(500);
CIntegerParameter(nodemap, "AutoFunctionROIHeight").SetValue(400);
// Enable Balance White Auto for the auto function ROI selected
CBooleanParameter(nodemap, "AutoFunctionROIUseWhiteBalance").SetValue(true);
// Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
CBooleanParameter(nodemap, "AutoFunctionROIUseBrightness").SetValue(true);
// Select auto function ROI 1
camera.Parameters[PLCamera.AutoFunctionROISelector].SetValue(PLCamera.AutoFunctionROISelector.ROI1);
// Specify position and size of the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionROIOffsetX].SetValue(10);
camera.Parameters[PLCamera.AutoFunctionROIOffsetY].SetValue(10);
camera.Parameters[PLCamera.AutoFunctionROIWidth].SetValue(500);
camera.Parameters[PLCamera.AutoFunctionROIHeight].SetValue(400);
// Enable Balance White Auto for the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionROIUseWhiteBalance].SetValue(true);
// Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionROIUseBrightness].SetValue(true);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Select auto function ROI 1 */
errRes = PylonDeviceFeatureFromString(hdev, "AutoFunctionROISelector", "ROI1");
CHECK(errRes);
/* Specify position and size of the auto function ROI selected */
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionROIOffsetX", 10);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionROIOffsetY", 10);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionROIWidth", 500);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoFunctionROIHeight", 400);
CHECK(errRes);
/* Enable Balance White Auto for the auto function ROI selected */
errRes = PylonDeviceSetBooleanFeature(hdev, "AutoFunctionROIUseWhiteBalance", 1);
CHECK(errRes);
/* Enable the 'Brightness' auto function (Gain Auto + Exposure Auto) */
/* for the auto function ROI selected */
errRes = PylonDeviceSetBooleanFeature(hdev, "AutoFunctionROIUseBrightness", 1);
CHECK(errRes);
# Select auto function ROI 1
camera.AutoFunctionROISelector.Value = "ROI1"
# Specify position and size of the auto function ROI selected
camera.AutoFunctionROIOffsetX.Value = 10
camera.AutoFunctionROIOffsetY.Value = 10
camera.AutoFunctionROIWidth.Value = 500
camera.AutoFunctionROIHeight.Value = 400
# Enable Balance White Auto for the auto function ROI selected
camera.AutoFunctionROIUseWhiteBalance.Value = True
# Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
# for the auto function ROI selected
camera.AutoFunctionROIUseBrightness.Value = True
You can also use the pylon Viewer to easily set the parameters.