Web Server Enable#
The web server must be enabled if you want to update the firmware or download status and diagnostic information from the camera. By default, it is enabled.
Info
You can generate the diagnostic archive while the web server is disabled. However, to be able to download it, the web server must be running. To learn how to generate status and diagnostic information, see the Diagnostic Information topic.
To enable the web server:
- Set the
WebServerEnable
parameter totrue
. - Power-cycle the camera for the change to become effective.
Info
Changes to this value are persisted automatically.