Skip to content

Color Adjustment#

The Color Adjustment camera feature allows you to adjust the hue and saturation of individual colors in your images.

You can adjust hue and saturation separately for each primary and secondary color in the RGB color space (red, green, blue, yellow, cyan, and magenta).

If you want to adjust the appearance of all colors in a single step, use the Hue and Saturation feature (if available).

Using the Feature#

Why Use Color Adjustment#

  • Adjusting the hue shifts the colors of the image. This can be useful, e.g., to correct minor, undesirable, color shifts or to create false-color images.
  • Adjusting the saturation changes the colorfulness (intensity) of the colors. Increasing the saturation can be useful to make colors easier to distinguish.

Setting the Color Adjustment Parameters#

  1. Set the ProcessedRawEnable parameter to true (if available and if you're using a Bayer pixel format).
  2. Set the ColorAdjustmentEnable parameter to true (if available).
  3. Set the ColorAdjustmentSelector parameter to the desired color, e.g., Red.
  4. Enter the desired value for the ColorAdjustmentHue parameter. When the parameter is set to 0, the hue is not changed.
  5. Enter the desired value for the ColorAdjustmentSaturation parameter. When the parameter is set to 1, the saturation is not changed.

How It Works#

The parameters of the Color Adjustment feature refer to the RGB color cube.

For easier visualization, the color cube can be projected onto a plane, resulting in a color hexagon:

RGB Color Cube Projected On a Plane

The primary colors (red, green, blue) and the secondary colors (yellow, cyan, magenta) are placed at the corners of this color hexagon.

You can adjust hue and saturation for each of these colors. This affects all areas in the image where the adjusted color predominates. For example, adjusting red affects the colors in the image with a predominantly red component.

The following diagram shows how changing hue and saturation of the color red affects the colors of your images:

Hue and Saturation Adjustment In the Color Hexagon. Adjustments Are Indicated for Red as an Example

The following effects become apparent:

If the value range of the ColorAdjustmentHue parameter is -4.0 to 3.96875:

  • Decreasing the hue changes all red colors (i.e., colors with a predominantly red component) towards yellow.
  • Increasing the hue changes all red colors towards magenta.

If the value range of the ColorAdjustmentHue parameter is -1.0 to 1.0:

  • Increasing the hue changes all red colors (i.e., colors with a predominantly red component) towards yellow.
  • Decreasing the hue changes all red colors towards magenta.

Decreasing the saturation decreases the colorfulness of all red colors. At minimum, all red colors will be replaced by gray.

Increasing the saturation increases the colorfulness of all red colors. At maximum, all red colors are replaced by 100 % red.

Info

When you adjust a color, the nearest neighboring colors in the color hexagon will also be affected to some degree. For example, when you adjust red, yellow and magenta will also be affected.

Additional Parameters#

Depending on your camera model, the following additional parameters are available:

  • ColorAdjustmentEnable: Enables or disables the Color Adjustment feature.
  • ColorAdjustmentReset command: Allows you to reset the color adjustment parameters to their initial values. This is especially useful if your adjustments haven't had the desired effect and you want to return quickly to the original settings.
  • ColorAdjustmentHueRaw: Allows you to enter integer values ranging from -128 to 127 for the hue parameter. The integer range maps linearly to the floating point range with -128 being equivalent to -4.0, 32 being equivalent to 1.0, and 127 being equivalent to 3.96875.
  • ColorAdjustmentSaturationRaw: Allows you to enter integer values ranging from 0 to 255 for the saturation parameter. The integer range maps linearly to the floating point range with 0 being equivalent to 0.0, 128 being equivalent to 1.0, and 255 being equivalent to 1.99219.

Specifics#

Show all camera models

Camera Model Additional Parameters
a2A640-240gmSWIR Color Adjustment feature not supported
a2A640-240umSWIR Color Adjustment feature not supported
a2A1280-80gmSWIR Color Adjustment feature not supported
a2A1280-125umSWIR Color Adjustment feature not supported
a2A1920-51gcBAS BslColorAdjustmentEnable
a2A1920-51gcPRO BslColorAdjustmentEnable
a2A1920-51gmBAS Color Adjustment feature not supported
a2A1920-51gmPRO Color Adjustment feature not supported
a2A1920-160ucBAS BslColorAdjustmentEnable
a2A1920-160ucPRO BslColorAdjustmentEnable
a2A1920-160umBAS Color Adjustment feature not supported
a2A1920-160umPRO Color Adjustment feature not supported
a2A1920-165g5cBAS BslColorAdjustmentEnable
a2A1920-165g5mBAS Color Adjustment feature not supported
a2A2048-35gmSWIR Color Adjustment feature not supported
a2A2048-37gcBAS BslColorAdjustmentEnable
a2A2048-37gcPRO BslColorAdjustmentEnable
a2A2048-37gmBAS Color Adjustment feature not supported
a2A2048-37gmPRO Color Adjustment feature not supported
a2A2048-110umSWIR Color Adjustment feature not supported
a2A2048-114g5cBAS BslColorAdjustmentEnable
a2A2048-114g5mBAS Color Adjustment feature not supported
a2A2048-114ucBAS BslColorAdjustmentEnable
a2A2048-114ucPRO BslColorAdjustmentEnable
a2A2048-114umBAS Color Adjustment feature not supported
a2A2048-114umPRO Color Adjustment feature not supported
a2A2440-98g5cBAS BslColorAdjustmentEnable
a2A2440-98g5mBAS Color Adjustment feature not supported
a2A2448-23gcBAS BslColorAdjustmentEnable
a2A2448-23gcPRO BslColorAdjustmentEnable
a2A2448-23gmBAS Color Adjustment feature not supported
a2A2448-23gmPRO Color Adjustment feature not supported
a2A2448-75ucBAS BslColorAdjustmentEnable
a2A2448-75ucPRO BslColorAdjustmentEnable
a2A2448-75umBAS Color Adjustment feature not supported
a2A2448-75umPRO Color Adjustment feature not supported
a2A2448-105g5cBAS BslColorAdjustmentEnable
a2A2448-105g5mBAS Color Adjustment feature not supported
a2A2448-120cc BslColorAdjustmentEnable
a2A2448-120cm Color Adjustment feature not supported
a2A2448-210cc BslColorAdjustmentEnable
a2A2448-210cm Color Adjustment feature not supported
a2A2560-20gmSWIR Color Adjustment feature not supported
a2A2560-70umSWIR Color Adjustment feature not supported
a2A2590-22gcBAS BslColorAdjustmentEnable
a2A2590-22gcPRO BslColorAdjustmentEnable
a2A2590-22gmBAS Color Adjustment feature not supported
a2A2590-22gmPRO Color Adjustment feature not supported
a2A2590-60ucBAS BslColorAdjustmentEnable
a2A2590-60ucPRO BslColorAdjustmentEnable
a2A2590-60umBAS Color Adjustment feature not supported
a2A2590-60umPRO Color Adjustment feature not supported
a2A2600-20gcBAS BslColorAdjustmentEnable
a2A2600-20gcPRO BslColorAdjustmentEnable
a2A2600-20gmBAS Color Adjustment feature not supported
a2A2600-20gmPRO Color Adjustment feature not supported
a2A2600-64ucBAS BslColorAdjustmentEnable
a2A2600-64ucPRO BslColorAdjustmentEnable
a2A2600-64umBAS Color Adjustment feature not supported
a2A2600-64umPRO Color Adjustment feature not supported
a2A2840-14gcBAS BslColorAdjustmentEnable
a2A2840-14gcPRO BslColorAdjustmentEnable
a2A2840-14gmBAS Color Adjustment feature not supported
a2A2840-14gmPRO Color Adjustment feature not supported
a2A2840-14gmUV Color Adjustment feature not supported
a2A2840-48ucBAS BslColorAdjustmentEnable
a2A2840-48ucPRO BslColorAdjustmentEnable
a2A2840-48umBAS Color Adjustment feature not supported
a2A2840-48umPRO Color Adjustment feature not supported
a2A2840-48umUV Color Adjustment feature not supported
a2A2840-67g5cBAS BslColorAdjustmentEnable
a2A2840-67g5mBAS Color Adjustment feature not supported
a2A2840-67g5mUV Color Adjustment feature not supported
a2A2840-86cc BslColorAdjustmentEnable
a2A2840-86cm Color Adjustment feature not supported
a2A3536-9gcBAS BslColorAdjustmentEnable
a2A3536-9gcPRO BslColorAdjustmentEnable
a2A3536-9gmBAS Color Adjustment feature not supported
a2A3536-9gmPRO Color Adjustment feature not supported
a2A3536-31ucBAS BslColorAdjustmentEnable
a2A3536-31ucPRO BslColorAdjustmentEnable
a2A3536-31umBAS Color Adjustment feature not supported
a2A3536-31umPRO Color Adjustment feature not supported
a2A3536-42g5cBAS BslColorAdjustmentEnable
a2A3536-42g5mBAS Color Adjustment feature not supported
a2A3840-13gcBAS BslColorAdjustmentEnable
a2A3840-13gcPRO BslColorAdjustmentEnable
a2A3840-13gmBAS Color Adjustment feature not supported
a2A3840-13gmPRO Color Adjustment feature not supported
a2A3840-45ucBAS BslColorAdjustmentEnable
a2A3840-45ucPRO BslColorAdjustmentEnable
a2A3840-45umBAS Color Adjustment feature not supported
a2A3840-45umPRO Color Adjustment feature not supported
a2A4096-9gcBAS BslColorAdjustmentEnable
a2A4096-9gcPRO BslColorAdjustmentEnable
a2A4096-9gmBAS Color Adjustment feature not supported
a2A4096-9gmPRO Color Adjustment feature not supported
a2A4096-30ucBAS BslColorAdjustmentEnable
a2A4096-30ucPRO BslColorAdjustmentEnable
a2A4096-30umBAS Color Adjustment feature not supported
a2A4096-30umPRO Color Adjustment feature not supported
a2A4096-44g5cBAS BslColorAdjustmentEnable
a2A4096-44g5mBAS Color Adjustment feature not supported
a2A4096-67cc BslColorAdjustmentEnable
a2A4096-67cm Color Adjustment feature not supported
a2A4200-12gcBAS BslColorAdjustmentEnable
a2A4200-12gcPRO BslColorAdjustmentEnable
a2A4200-12gmBAS Color Adjustment feature not supported
a2A4200-12gmPRO Color Adjustment feature not supported
a2A4200-40ucBAS BslColorAdjustmentEnable
a2A4200-40ucPRO BslColorAdjustmentEnable
a2A4200-40umBAS Color Adjustment feature not supported
a2A4200-40umPRO Color Adjustment feature not supported
a2A4504-5gcBAS BslColorAdjustmentEnable
a2A4504-5gcPRO BslColorAdjustmentEnable
a2A4504-5gmBAS Color Adjustment feature not supported
a2A4504-5gmPRO Color Adjustment feature not supported
a2A4504-18ucBAS BslColorAdjustmentEnable
a2A4504-18ucPRO BslColorAdjustmentEnable
a2A4504-18umBAS Color Adjustment feature not supported
a2A4504-18umPRO Color Adjustment feature not supported
a2A4504-27g5cBAS BslColorAdjustmentEnable
a2A4504-27g5mBAS Color Adjustment feature not supported
a2A4504-42cc BslColorAdjustmentEnable
a2A4504-42cm Color Adjustment feature not supported
a2A4508-6gcBAS BslColorAdjustmentEnable
a2A4508-6gcPRO BslColorAdjustmentEnable
a2A4508-6gmBAS Color Adjustment feature not supported
a2A4508-6gmPRO Color Adjustment feature not supported
a2A4508-20ucBAS BslColorAdjustmentEnable
a2A4508-20ucPRO BslColorAdjustmentEnable
a2A4508-20umBAS Color Adjustment feature not supported
a2A4508-20umPRO Color Adjustment feature not supported
a2A5060-4gcBAS BslColorAdjustmentEnable
a2A5060-4gmBAS Color Adjustment feature not supported
a2A5060-15ucBAS BslColorAdjustmentEnable
a2A5060-15umBAS Color Adjustment feature not supported
a2A5060-21g5cBAS BslColorAdjustmentEnable
a2A5060-21g5mBAS Color Adjustment feature not supported
a2A5060-35cc BslColorAdjustmentEnable
a2A5060-35cm Color Adjustment feature not supported
a2A5320-7gcBAS BslColorAdjustmentEnable
a2A5320-7gcPRO BslColorAdjustmentEnable
a2A5320-7gmBAS Color Adjustment feature not supported
a2A5320-7gmPRO Color Adjustment feature not supported
a2A5320-23ucBAS BslColorAdjustmentEnable
a2A5320-23ucPRO BslColorAdjustmentEnable
a2A5320-23umBAS Color Adjustment feature not supported
a2A5320-23umPRO Color Adjustment feature not supported
a2A5320-34g5cBAS BslColorAdjustmentEnable
a2A5320-34g5mBAS Color Adjustment feature not supported
a2A5320-52cc BslColorAdjustmentEnable
a2A5320-52cm Color Adjustment feature not supported
a2A5328-4gcBAS BslColorAdjustmentEnable
a2A5328-4gcPRO BslColorAdjustmentEnable
a2A5328-4gmBAS Color Adjustment feature not supported
a2A5328-4gmPRO Color Adjustment feature not supported
a2A5328-15ucBAS BslColorAdjustmentEnable
a2A5328-15ucPRO BslColorAdjustmentEnable
a2A5328-15umBAS Color Adjustment feature not supported
a2A5328-15umPRO Color Adjustment feature not supported
a2A5328-22g5cBAS BslColorAdjustmentEnable
a2A5328-22g5mBAS Color Adjustment feature not supported
a2A5328-35cc BslColorAdjustmentEnable
a2A5328-35cm Color Adjustment feature not supported
acA640-121gm Color Adjustment feature not supported
acA640-300gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA640-300gm Color Adjustment feature not supported
acA640-750uc None
acA640-750um Color Adjustment feature not supported
acA720-290gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA720-290gm Color Adjustment feature not supported
acA720-520uc None
acA720-520um Color Adjustment feature not supported
acA800-200gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA800-200gm Color Adjustment feature not supported
acA800-510uc None
acA800-510um Color Adjustment feature not supported
acA1280-60gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA1280-60gm Color Adjustment feature not supported
acA1300-60gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA1300-60gm Color Adjustment feature not supported
acA1300-60gmNIR Color Adjustment feature not supported
acA1300-75gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA1300-75gm Color Adjustment feature not supported
acA1300-200uc None
acA1300-200um Color Adjustment feature not supported
acA1440-73gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA1440-73gm Color Adjustment feature not supported
acA1440-220uc None
acA1440-220um Color Adjustment feature not supported
acA1600-20gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA1600-20uc None
acA1600-60gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA1600-60gm Color Adjustment feature not supported
acA1920-25gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA1920-25gm Color Adjustment feature not supported
acA1920-25uc None
acA1920-25um Color Adjustment feature not supported
acA1920-40gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA1920-40gm Color Adjustment feature not supported
acA1920-40uc None
acA1920-40ucMED None
acA1920-40um Color Adjustment feature not supported
acA1920-40umMED Color Adjustment feature not supported
acA1920-48gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA1920-48gm Color Adjustment feature not supported
acA1920-50gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA1920-50gm Color Adjustment feature not supported
acA1920-150uc None
acA1920-150um Color Adjustment feature not supported
acA1920-155uc None
acA1920-155ucMED None
acA1920-155um Color Adjustment feature not supported
acA1920-155umMED Color Adjustment feature not supported
acA2000-50gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA2000-50gm Color Adjustment feature not supported
acA2000-165uc Color Adjustment feature not supported
acA2000-165um Color Adjustment feature not supported
acA2040-25gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA2040-25gm Color Adjustment feature not supported
acA2040-25gmNIR Color Adjustment feature not supported
acA2040-35gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA2040-35gm Color Adjustment feature not supported
acA2040-55uc None
acA2040-55um Color Adjustment feature not supported
acA2040-90uc Color Adjustment feature not supported
acA2040-90um Color Adjustment feature not supported
acA2040-90umNIR Color Adjustment feature not supported
acA2040-120uc None
acA2040-120um Color Adjustment feature not supported
acA2440-20gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA2440-20gm Color Adjustment feature not supported
acA2440-35uc None
acA2440-35ucMED None
acA2440-35um Color Adjustment feature not supported
acA2440-35umMED Color Adjustment feature not supported
acA2440-75uc None
acA2440-75ucMED None
acA2440-75um Color Adjustment feature not supported
acA2440-75umMED Color Adjustment feature not supported
acA2500-14gc Color Adjustment feature not supported
acA2500-14gm Color Adjustment feature not supported
acA2500-14uc None
acA2500-14um Color Adjustment feature not supported
acA2500-20gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA2500-20gcMED ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA2500-20gm Color Adjustment feature not supported
acA2500-20gmMED Color Adjustment feature not supported
acA2500-60uc None
acA2500-60um Color Adjustment feature not supported
acA3088-16gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA3088-16gm Color Adjustment feature not supported
acA3088-57uc None
acA3088-57ucMED None
acA3088-57um Color Adjustment feature not supported
acA3088-57umMED Color Adjustment feature not supported
acA3800-10gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA3800-10gm Color Adjustment feature not supported
acA3800-14uc None
acA3800-14um Color Adjustment feature not supported
acA4024-8gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA4024-8gm Color Adjustment feature not supported
acA4024-29uc None
acA4024-29um Color Adjustment feature not supported
acA4096-11gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA4096-11gm Color Adjustment feature not supported
acA4096-30uc None
acA4096-30ucMED None
acA4096-30um Color Adjustment feature not supported
acA4096-30umMED Color Adjustment feature not supported
acA4096-40uc None
acA4096-40ucMED None
acA4096-40um Color Adjustment feature not supported
acA4096-40umMED Color Adjustment feature not supported
acA4112-8gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA4112-8gm Color Adjustment feature not supported
acA4112-20uc None
acA4112-20ucMED None
acA4112-20um Color Adjustment feature not supported
acA4112-20umMED Color Adjustment feature not supported
acA4112-30uc None
acA4112-30ucMED None
acA4112-30um Color Adjustment feature not supported
acA4112-30umMED Color Adjustment feature not supported
acA5472-5gc ColorAdjustmentEnable[^a]
ColorAdjustmentReset
ColorAdjustmentHueRaw
ColorAdjustmentSaturationRaw
acA5472-5gm Color Adjustment feature not supported
acA5472-17uc None
acA5472-17ucMED None
acA5472-17um Color Adjustment feature not supported
acA5472-17umMED Color Adjustment feature not supported
boA1936-400cc BslColorAdjustmentEnable
boA1936-400cm Color Adjustment feature not supported
boA2448-250cc BslColorAdjustmentEnable
boA2448-250cm Color Adjustment feature not supported
boA2832-190cc BslColorAdjustmentEnable
boA2832-190cm Color Adjustment feature not supported
boA4096-93cc BslColorAdjustmentEnable
boA4096-93cm Color Adjustment feature not supported
boA4096-180cc BslColorAdjustmentEnable
boA4096-180cm Color Adjustment feature not supported
boA4112-68cc BslColorAdjustmentEnable
boA4112-68cm Color Adjustment feature not supported
boA4500-45cc BslColorAdjustmentEnable
boA4500-45cm Color Adjustment feature not supported
boA4504-100cc BslColorAdjustmentEnable
boA4504-100cm Color Adjustment feature not supported
boA5120-150cc Color Adjustment feature not supported
boA5120-150cm Color Adjustment feature not supported
boA5120-230cc Color Adjustment feature not supported
boA5120-230cm Color Adjustment feature not supported
boA5320-150cc BslColorAdjustmentEnable
boA5320-150cm Color Adjustment feature not supported
boA5328-100cc BslColorAdjustmentEnable
boA5328-100cm Color Adjustment feature not supported
boA6500-36cc BslColorAdjustmentEnable
boA6500-36cm Color Adjustment feature not supported
boA8100-16cc BslColorAdjustmentEnable
boA8100-16cm Color Adjustment feature not supported
boA9344-30cc Color Adjustment feature not supported
boA9344-30cm Color Adjustment feature not supported
boA9344-70cc Color Adjustment feature not supported
boA9344-70cm Color Adjustment feature not supported
boA13440-17cm Color Adjustment feature not supported
daA720-520uc Color Adjustment feature not supported
daA720-520um Color Adjustment feature not supported
daA1280-54uc Color Adjustment feature not supported
daA1280-54um Color Adjustment feature not supported
daA1440-220uc Color Adjustment feature not supported
daA1440-220um Color Adjustment feature not supported
daA1600-60uc Color Adjustment feature not supported
daA1600-60um Color Adjustment feature not supported
daA1920-15um Color Adjustment feature not supported
daA1920-30uc Color Adjustment feature not supported
daA1920-30um Color Adjustment feature not supported
daA1920-160uc Color Adjustment feature not supported
daA1920-160um Color Adjustment feature not supported
daA2448-70uc Color Adjustment feature not supported
daA2448-70um Color Adjustment feature not supported
daA2500-14uc Color Adjustment feature not supported
daA2500-14um Color Adjustment feature not supported
daA3840-45uc Color Adjustment feature not supported
daA3840-45um Color Adjustment feature not supported
dmA720-290gc BslColorAdjustmentEnable
dmA720-290gm Color Adjustment feature not supported
dmA1440-73gc BslColorAdjustmentEnable
dmA1440-73gm Color Adjustment feature not supported
dmA1920-51gc BslColorAdjustmentEnable
dmA1920-51gm Color Adjustment feature not supported
dmA2048-37gc BslColorAdjustmentEnable
dmA2048-37gm Color Adjustment feature not supported
dmA2448-23gc BslColorAdjustmentEnable
dmA2448-23gm Color Adjustment feature not supported
dmA2840-14gc BslColorAdjustmentEnable
dmA2840-14gm Color Adjustment feature not supported
dmA3536-9gc BslColorAdjustmentEnable
dmA3536-9gm Color Adjustment feature not supported
dmA4096-9gc BslColorAdjustmentEnable
dmA4096-9gm Color Adjustment feature not supported
puA1280-54uc Color Adjustment feature not supported
puA1280-54um Color Adjustment feature not supported
puA1600-60uc Color Adjustment feature not supported
puA1600-60um Color Adjustment feature not supported
puA1920-30uc Color Adjustment feature not supported
puA1920-30um Color Adjustment feature not supported
puA2500-14uc Color Adjustment feature not supported
puA2500-14um Color Adjustment feature not supported
r2L2048-29gc BslColorAdjustmentEnable
r2L2048-58gm Color Adjustment feature not supported
r2L2048-62cc BslColorAdjustmentEnable
r2L2048-62g5c BslColorAdjustmentEnable
r2L2048-172cm Color Adjustment feature not supported
r2L2048-172g5m Color Adjustment feature not supported
r2L4096-14gc BslColorAdjustmentEnable
r2L4096-29gm Color Adjustment feature not supported
r2L4096-42cc BslColorAdjustmentEnable
r2L4096-42g5c BslColorAdjustmentEnable
r2L4096-84cm Color Adjustment feature not supported
r2L4096-84g5m Color Adjustment feature not supported
r2L8192-200cm Color Adjustment feature not supported
r2L16384-120cm Color Adjustment feature not supported

Sample Code#

ace Classic/U/L GigE Cameras#
// Enable the Color Adjustment feature
camera.ColorAdjustmentEnable.SetValue(true);
// Select red as the color to adjust
camera.ColorAdjustmentSelector.SetValue(ColorAdjustmentSelector_Red);
// Enter a floating point value for the red hue
camera.ColorAdjustmentHue.SetValue(-1.125);
// Enter a floating point value for the red saturation
camera.ColorAdjustmentSaturation.SetValue(1.375);
// Select cyan as the color to adjust
camera.ColorAdjustmentSelector.SetValue(ColorAdjustmentSelector_Cyan);
// Enter an integer value for the cyan hue
camera.ColorAdjustmentHueRaw.SetValue(-36);
// Enter an integer value for the cyan saturation
camera.ColorAdjustmentSaturationRaw.SetValue(176);
INodeMap& nodemap = camera.GetNodeMap();
// Enable the Color Adjustment feature
CBooleanParameter(nodemap, "ColorAdjustmentEnable").SetValue(true);
// Select red as the color to adjust
CEnumParameter(nodemap, "ColorAdjustmentSelector").SetValue("Red");
// Enter a floating point value for the red hue
CFloatParameter(nodemap, "ColorAdjustmentHue").SetValue(-1.125);
// Enter a floating point value for the red saturation
CFloatParameter(nodemap, "ColorAdjustmentSaturation").SetValue(1.375);
// Select cyan as the color to adjust
CEnumParameter(nodemap, "ColorAdjustmentSelector").SetValue("Cyan");
// Enter an integer value for the cyan hue
CIntegerParameter(nodemap, "ColorAdjustmentHueRaw").SetValue(-36);
// Enter an integer value for the cyan saturation
CIntegerParameter(nodemap, "ColorAdjustmentSaturationRaw").SetValue(176);
// Enable the Color Adjustment feature
camera.Parameters[PLCamera.ColorAdjustmentEnable].SetValue(true);
// Select red as the color to adjust
camera.Parameters[PLCamera.ColorAdjustmentSelector].SetValue(PLCamera.ColorAdjustmentSelector.Red);
// Enter a floating point value for the red hue
camera.Parameters[PLCamera.ColorAdjustmentHue].SetValue(-1.125);
// Enter a floating point value for the red saturation
camera.Parameters[PLCamera.ColorAdjustmentSaturation].SetValue(1.375);
// Select cyan as the color to adjust
camera.Parameters[PLCamera.ColorAdjustmentSelector].SetValue(PLCamera.ColorAdjustmentSelector.Cyan);
// Enter an integer value for the cyan hue
camera.Parameters[PLCamera.ColorAdjustmentHueRaw].SetValue(-36);
// Enter an integer value for the cyan saturation
camera.Parameters[PLCamera.ColorAdjustmentSaturationRaw].SetValue(176);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Enable the Color Adjustment feature */
errRes = PylonDeviceSetBooleanFeature(hdev, "ColorAdjustmentEnable", 1);
CHECK(errRes);
/* Select red as the color to adjust */
errRes = PylonDeviceFeatureFromString(hdev, "ColorAdjustmentSelector", "Red");
CHECK(errRes);
/* Enter a floating point value for the red hue */
errRes = PylonDeviceSetFloatFeature(hdev, "ColorAdjustmentHue", -1.125);
CHECK(errRes);
/* Enter a floating point value for the red saturation */
errRes = PylonDeviceSetFloatFeature(hdev, "ColorAdjustmentSaturation", 1.375);
CHECK(errRes);
/* Select cyan as the color to adjust */
errRes = PylonDeviceFeatureFromString(hdev, "ColorAdjustmentSelector", "Cyan");
CHECK(errRes);
/* Enter an integer value for the cyan hue */
errRes = PylonDeviceSetIntegerFeature(hdev, "ColorAdjustmentHueRaw", -36);
CHECK(errRes);
/* Enter an integer value for the cyan saturation */
errRes = PylonDeviceSetIntegerFeature(hdev, "ColorAdjustmentSaturationRaw", 176);
CHECK(errRes);
# Enable the Color Adjustment feature
camera.ColorAdjustmentEnable.Value = True
# Select red as the color to adjust
camera.ColorAdjustmentSelector.Value = "Red"
# Enter a floating point value for the red hue
camera.ColorAdjustmentHue.Value = -1.125
# Enter a floating point value for the red saturation
camera.ColorAdjustmentSaturation.Value = 1.375
# Select cyan as the color to adjust
camera.ColorAdjustmentSelector.Value = "Cyan"
# Enter an integer value for the cyan hue
camera.ColorAdjustmentHueRaw.Value = -36
# Enter an integer value for the cyan saturation
camera.ColorAdjustmentSaturationRaw.Value = 176
ace 2, boost, and dart R Cameras#
// Select red as the color to adjust
camera.BslColorAdjustmentSelector.SetValue(ColorAdjustmentSelector_Red);
// Enter an integer value for the red hue
camera.BslColorAdjustmentHue.SetValue(-1.125);
// Enter an integer value for the red saturation
camera.BslColorAdjustmentSaturation.SetValue(1.375);
INodeMap& nodemap = camera.GetNodeMap();
// Select red as the color to adjust
CEnumParameter(nodemap, "BslColorAdjustmentSelector").SetValue("Red");
// Enter an integer value for the red hue
CFloatParameter(nodemap, "BslColorAdjustmentHue").SetValue(-1.125);
// Enter an integer value for the red saturation
CFloatParameter(nodemap, "BslColorAdjustmentSaturation").SetValue(1.375);
// Select red as the color to adjust
camera.Parameters[PLCamera.BslColorAdjustmentSelector].SetValue(PLCamera.ColorAdjustmentSelector.Red);
// Enter an integer value for the red hue
camera.Parameters[PLCamera.BslColorAdjustmentHue].SetValue(-1.125);
// Enter an integer value for the red saturation
camera.Parameters[PLCamera.BslColorAdjustmentSaturation].SetValue(1.375);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Select red as the color to adjust */
errRes = PylonDeviceFeatureFromString(hdev, "BslColorAdjustmentSelector", "Red");
CHECK(errRes);
/* Enter an integer value for the red hue */
errRes = PylonDeviceSetFloatFeature(hdev, "BslColorAdjustmentHue", -1.125);
CHECK(errRes);
/* Enter an integer value for the red saturation */
errRes = PylonDeviceSetFloatFeature(hdev, "BslColorAdjustmentSaturation", 1.375);
CHECK(errRes);
# Select red as the color to adjust
camera.BslColorAdjustmentSelector.Value = "Red"
# Enter an integer value for the red hue
camera.BslColorAdjustmentHue.Value = -1.125
# Enter an integer value for the red saturation
camera.BslColorAdjustmentSaturation.Value = 1.375
Other Cameras#
// Select red as the color to adjust
camera.ColorAdjustmentSelector.SetValue(ColorAdjustmentSelector_Red);
// Enter an integer value for the red hue
camera.ColorAdjustmentHue.SetValue(-1.125);
// Enter an integer value for the red saturation
camera.ColorAdjustmentSaturation.SetValue(1.375);
INodeMap& nodemap = camera.GetNodeMap();
// Select red as the color to adjust
CEnumParameter(nodemap, "ColorAdjustmentSelector").SetValue("Red");
// Enter an integer value for the red hue
CFloatParameter(nodemap, "ColorAdjustmentHue").SetValue(-1.125);
// Enter an integer value for the red saturation
CFloatParameter(nodemap, "ColorAdjustmentSaturation").SetValue(1.375);
// Select red as the color to adjust
camera.Parameters[PLCamera.ColorAdjustmentSelector].SetValue(PLCamera.ColorAdjustmentSelector.Red);
// Enter an integer value for the red hue
camera.Parameters[PLCamera.ColorAdjustmentHue].SetValue(-1.125);
// Enter an integer value for the red saturation
camera.Parameters[PLCamera.ColorAdjustmentSaturation].SetValue(1.375);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Select red as the color to adjust */
errRes = PylonDeviceFeatureFromString(hdev, "ColorAdjustmentSelector", "Red");
CHECK(errRes);
/* Enter an integer value for the red hue */
errRes = PylonDeviceSetFloatFeature(hdev, "ColorAdjustmentHue", -1.125);
CHECK(errRes);
/* Enter an integer value for the red saturation */
errRes = PylonDeviceSetFloatFeature(hdev, "ColorAdjustmentSaturation", 1.375);
CHECK(errRes);
# Select red as the color to adjust
camera.ColorAdjustmentSelector.Value = "Red"
# Enter an integer value for the red hue
camera.ColorAdjustmentHue.Value = -1.125
# Enter an integer value for the red saturation
camera.ColorAdjustmentSaturation.Value = 1.375

You can also use the pylon Viewer to easily set the parameters.