Skip to content

Features#

Features are capabilities of Basler cameras and camera modules that can be controlled by configuring firmware parameters.

You can configure the parameters via the Basler pylon API or via the Basler pylon Viewer.

Which Features Are Available for My Camera?#

To find out which features are available for a specific camera model:

  1. Select your camera model using the "Your camera model" filter at the top right corner of this page.
  2. Check the entries in the "Features" section in the table of contents. The color of the entries indicates whether a feature is available:

    Camera Features Availability

    (1) Feature is supported by the camera model currently selected.
    (2) Feature is not supported by the camera model currently selected.

Which Features Are Available for Any Basler Camera?#

For an overview, see the Basler Features Check List.