Skip to content

HDR (High Dynamic Range)#

HDR (High Dynamic Range) is an imaging technology that improves the brightness and contrast of an image.

HDR images show details within the image rather exactly, which makes them ideal for high-resolution image processing.

Using the Feature#

The dynamic range of an image is the ratio between the highest and lowest brightness that can be displayed. Images with a wide dynamic range capture the actual contrast of the scene very well, so more details in dark and light sections can bee seen.

HDR allows capturing a wider dynamic range by acquiring images with different exposures.

Interleaved HDR#

Some camera models, support interleaved HDR (iHDR). The iHDR feature allows you to set different exposure times for even and odd pixel lines of the sensor. For example, you can specify a long exposure time for lines 1, 3, 5, etc. and a reduced exposure time for lines 2, 4, 6, etc. The different exposures start simultaneously. This creates a "striped" image with bright and dark lines.

The following drawing visualizes the different exposures per sensor line.

iHDR Sensor Pixel Lines

To set the exposure times for iHDR:

  1. Set the ExposureTimeMode parameter to Individual.
  2. Set the ExposureTimeSelector parameter to Stage 1.
  3. Specify the exposure time for stage 1.
    The value specified for stage 1 applies to the even pixel lines of the sensor.
  4. Set the ExposureTimeSelector parameter to Stage 2.
  5. Specify the exposure time for stage 2.
    The value specified for stage 2 applies to the odd pixel lines of the sensor.

Info

You can find the minimum and maximum exposure time values of your camera model in the Specifics section of the Exposure Time topic.

Use an external post-processing program to combine the bright and dark lines to generate a high dynamic range image.

Quad HDR#

Some camera models support Quad HDR (QHDR). The QHDR feature allows you to set individual exposure times for pixels within pixel units. These are areas of 2×2 pixels, also called quad pixels, which includes two pixels in horizontal direction and two pixels in vertical direction.

Short and long exposures can be set for each of these four pixels included in each pixel unit. With this, you can extract the information in both the dark and bright regions of the image with every single image acquired.

The following drawing illustrates the different exposures per pixel unit:

QHDR Sensor Pixel Units

To set the exposure times for QHDR:

  1. Set the ExposureTimeMode parameter to Individual.
  2. Set the ExposureTimeSelector parameter to Stage 1.
  3. Specify the exposure time for stage 1.
  4. Repeat steps 2 and 3 for the other stages.

    The individual stages refer to the following pixels of each pixel unit:

    • Stage 1: The specified value applies to the upper left pixel.
    • Stage 2: The specified value applies to the upper right pixel.
    • Stage 3: The specified value applies to the lower left pixel.
    • Stage 4: The specified value applies to the lower right pixel.

    Info

    You can find the minimum and maximum exposure time values of your camera model in the Specifics section of the Exposure Time topic.

Use an external post-processing program to combine the information within each pixel unit to generate a high dynamic range image.

Specifics#

Show all camera models

Camera Model Available HDR Mode
a2A640-240gmSWIR HDR feature not supported
a2A640-240umSWIR HDR feature not supported
a2A1280-80gmSWIR HDR feature not supported
a2A1280-125umSWIR HDR feature not supported
a2A1920-51gcBAS HDR feature not supported
a2A1920-51gcPRO HDR feature not supported
a2A1920-51gmBAS HDR feature not supported
a2A1920-51gmPRO HDR feature not supported
a2A1920-160ucBAS HDR feature not supported
a2A1920-160ucPRO HDR feature not supported
a2A1920-160umBAS HDR feature not supported
a2A1920-160umPRO HDR feature not supported
a2A1920-165g5cBAS HDR feature not supported
a2A1920-165g5mBAS HDR feature not supported
a2A2048-35gmSWIR HDR feature not supported
a2A2048-37gcBAS HDR feature not supported
a2A2048-37gcPRO HDR feature not supported
a2A2048-37gmBAS Quad HDR
a2A2048-37gmPRO Quad HDR
a2A2048-110umSWIR HDR feature not supported
a2A2048-114g5cBAS HDR feature not supported
a2A2048-114g5mBAS Quad HDR
a2A2048-114ucBAS HDR feature not supported
a2A2048-114ucPRO HDR feature not supported
a2A2048-114umBAS Quad HDR
a2A2048-114umPRO Quad HDR
a2A2440-98g5cBAS HDR feature not supported
a2A2440-98g5mBAS HDR feature not supported
a2A2448-23gcBAS HDR feature not supported
a2A2448-23gcPRO HDR feature not supported
a2A2448-23gmBAS HDR feature not supported
a2A2448-23gmPRO HDR feature not supported
a2A2448-75ucBAS HDR feature not supported
a2A2448-75ucPRO HDR feature not supported
a2A2448-75umBAS HDR feature not supported
a2A2448-75umPRO HDR feature not supported
a2A2448-105g5cBAS HDR feature not supported
a2A2448-105g5mBAS HDR feature not supported
a2A2448-120cc HDR feature not supported
a2A2448-120cm HDR feature not supported
a2A2448-210cc HDR feature not supported
a2A2448-210cm HDR feature not supported
a2A2560-20gmSWIR HDR feature not supported
a2A2560-70umSWIR HDR feature not supported
a2A2590-22gcBAS HDR feature not supported
a2A2590-22gcPRO HDR feature not supported
a2A2590-22gmBAS HDR feature not supported
a2A2590-22gmPRO HDR feature not supported
a2A2590-60ucBAS HDR feature not supported
a2A2590-60ucPRO HDR feature not supported
a2A2590-60umBAS HDR feature not supported
a2A2590-60umPRO HDR feature not supported
a2A2600-20gcBAS HDR feature not supported
a2A2600-20gcPRO HDR feature not supported
a2A2600-20gmBAS Interleaved HDR
a2A2600-20gmPRO Interleaved HDR
a2A2600-64ucBAS HDR feature not supported
a2A2600-64ucPRO HDR feature not supported
a2A2600-64umBAS Interleaved HDR
a2A2600-64umPRO Interleaved HDR
a2A2840-14gcBAS HDR feature not supported
a2A2840-14gcPRO HDR feature not supported
a2A2840-14gmBAS HDR feature not supported
a2A2840-14gmPRO HDR feature not supported
a2A2840-14gmUV HDR feature not supported
a2A2840-48ucBAS HDR feature not supported
a2A2840-48ucPRO HDR feature not supported
a2A2840-48umBAS HDR feature not supported
a2A2840-48umPRO HDR feature not supported
a2A2840-48umUV HDR feature not supported
a2A2840-67g5cBAS HDR feature not supported
a2A2840-67g5mBAS HDR feature not supported
a2A2840-67g5mUV HDR feature not supported
a2A2840-86cc HDR feature not supported
a2A2840-86cm HDR feature not supported
a2A3536-9gcBAS HDR feature not supported
a2A3536-9gcPRO HDR feature not supported
a2A3536-9gmBAS HDR feature not supported
a2A3536-9gmPRO HDR feature not supported
a2A3536-31ucBAS HDR feature not supported
a2A3536-31ucPRO HDR feature not supported
a2A3536-31umBAS HDR feature not supported
a2A3536-31umPRO HDR feature not supported
a2A3536-42g5cBAS HDR feature not supported
a2A3536-42g5mBAS HDR feature not supported
a2A3840-13gcBAS HDR feature not supported
a2A3840-13gcPRO HDR feature not supported
a2A3840-13gmBAS HDR feature not supported
a2A3840-13gmPRO HDR feature not supported
a2A3840-45ucBAS HDR feature not supported
a2A3840-45ucPRO HDR feature not supported
a2A3840-45umBAS HDR feature not supported
a2A3840-45umPRO HDR feature not supported
a2A4096-9gcBAS HDR feature not supported
a2A4096-9gcPRO HDR feature not supported
a2A4096-9gmBAS HDR feature not supported
a2A4096-9gmPRO HDR feature not supported
a2A4096-30ucBAS HDR feature not supported
a2A4096-30ucPRO HDR feature not supported
a2A4096-30umBAS HDR feature not supported
a2A4096-30umPRO HDR feature not supported
a2A4096-44g5cBAS HDR feature not supported
a2A4096-44g5mBAS HDR feature not supported
a2A4096-67cc HDR feature not supported
a2A4096-67cm HDR feature not supported
a2A4200-12gcBAS HDR feature not supported
a2A4200-12gcPRO HDR feature not supported
a2A4200-12gmBAS Interleaved HDR
a2A4200-12gmPRO Interleaved HDR
a2A4200-40ucBAS HDR feature not supported
a2A4200-40ucPRO HDR feature not supported
a2A4200-40umBAS Interleaved HDR
a2A4200-40umPRO Interleaved HDR
a2A4504-5gcBAS HDR feature not supported
a2A4504-5gcPRO HDR feature not supported
a2A4504-5gmBAS HDR feature not supported
a2A4504-5gmPRO HDR feature not supported
a2A4504-18ucBAS HDR feature not supported
a2A4504-18ucPRO HDR feature not supported
a2A4504-18umBAS HDR feature not supported
a2A4504-18umPRO HDR feature not supported
a2A4504-27g5cBAS HDR feature not supported
a2A4504-27g5mBAS HDR feature not supported
a2A4504-42cc HDR feature not supported
a2A4504-42cm HDR feature not supported
a2A4508-6gcBAS HDR feature not supported
a2A4508-6gcPRO HDR feature not supported
a2A4508-6gmBAS Interleaved HDR
a2A4508-6gmPRO Interleaved HDR
a2A4508-20ucBAS HDR feature not supported
a2A4508-20ucPRO HDR feature not supported
a2A4508-20umBAS Interleaved HDR
a2A4508-20umPRO Interleaved HDR
a2A5060-4gcBAS HDR feature not supported
a2A5060-4gmBAS HDR feature not supported
a2A5060-15ucBAS HDR feature not supported
a2A5060-15umBAS HDR feature not supported
a2A5060-21g5cBAS HDR feature not supported
a2A5060-21g5mBAS HDR feature not supported
a2A5060-35cc HDR feature not supported
a2A5060-35cm HDR feature not supported
a2A5320-7gcBAS HDR feature not supported
a2A5320-7gcPRO HDR feature not supported
a2A5320-7gmBAS HDR feature not supported
a2A5320-7gmPRO HDR feature not supported
a2A5320-23ucBAS HDR feature not supported
a2A5320-23ucPRO HDR feature not supported
a2A5320-23umBAS HDR feature not supported
a2A5320-23umPRO HDR feature not supported
a2A5320-34g5cBAS HDR feature not supported
a2A5320-34g5mBAS HDR feature not supported
a2A5320-52cc HDR feature not supported
a2A5320-52cm HDR feature not supported
a2A5328-4gcBAS HDR feature not supported
a2A5328-4gcPRO HDR feature not supported
a2A5328-4gmBAS HDR feature not supported
a2A5328-4gmPRO HDR feature not supported
a2A5328-15ucBAS HDR feature not supported
a2A5328-15ucPRO HDR feature not supported
a2A5328-15umBAS HDR feature not supported
a2A5328-15umPRO HDR feature not supported
a2A5328-22g5cBAS HDR feature not supported
a2A5328-22g5mBAS HDR feature not supported
a2A5328-35cc HDR feature not supported
a2A5328-35cm HDR feature not supported
acA640-121gm HDR feature not supported
acA640-300gc HDR feature not supported
acA640-300gm HDR feature not supported
acA640-750uc HDR feature not supported
acA640-750um HDR feature not supported
acA720-290gc HDR feature not supported
acA720-290gm HDR feature not supported
acA720-520uc HDR feature not supported
acA720-520um HDR feature not supported
acA800-200gc HDR feature not supported
acA800-200gm HDR feature not supported
acA800-510uc HDR feature not supported
acA800-510um HDR feature not supported
acA1280-60gc HDR feature not supported
acA1280-60gm HDR feature not supported
acA1300-60gc HDR feature not supported
acA1300-60gm HDR feature not supported
acA1300-60gmNIR HDR feature not supported
acA1300-75gc HDR feature not supported
acA1300-75gm HDR feature not supported
acA1300-200uc HDR feature not supported
acA1300-200um HDR feature not supported
acA1440-73gc HDR feature not supported
acA1440-73gm HDR feature not supported
acA1440-220uc HDR feature not supported
acA1440-220um HDR feature not supported
acA1600-20gc HDR feature not supported
acA1600-20uc HDR feature not supported
acA1600-60gc HDR feature not supported
acA1600-60gm HDR feature not supported
acA1920-25gc HDR feature not supported
acA1920-25gm HDR feature not supported
acA1920-25uc HDR feature not supported
acA1920-25um HDR feature not supported
acA1920-40gc HDR feature not supported
acA1920-40gm HDR feature not supported
acA1920-40uc HDR feature not supported
acA1920-40ucMED HDR feature not supported
acA1920-40um HDR feature not supported
acA1920-40umMED HDR feature not supported
acA1920-48gc HDR feature not supported
acA1920-48gm HDR feature not supported
acA1920-50gc HDR feature not supported
acA1920-50gm HDR feature not supported
acA1920-150uc HDR feature not supported
acA1920-150um HDR feature not supported
acA1920-155uc HDR feature not supported
acA1920-155ucMED HDR feature not supported
acA1920-155um HDR feature not supported
acA1920-155umMED HDR feature not supported
acA2000-50gc HDR feature not supported
acA2000-50gm HDR feature not supported
acA2000-165uc HDR feature not supported
acA2000-165um HDR feature not supported
acA2040-25gc HDR feature not supported
acA2040-25gm HDR feature not supported
acA2040-25gmNIR HDR feature not supported
acA2040-35gc HDR feature not supported
acA2040-35gm HDR feature not supported
acA2040-55uc HDR feature not supported
acA2040-55um HDR feature not supported
acA2040-90uc HDR feature not supported
acA2040-90um HDR feature not supported
acA2040-90umNIR HDR feature not supported
acA2040-120uc HDR feature not supported
acA2040-120um HDR feature not supported
acA2440-20gc HDR feature not supported
acA2440-20gm HDR feature not supported
acA2440-35uc HDR feature not supported
acA2440-35ucMED HDR feature not supported
acA2440-35um HDR feature not supported
acA2440-35umMED HDR feature not supported
acA2440-75uc HDR feature not supported
acA2440-75ucMED HDR feature not supported
acA2440-75um HDR feature not supported
acA2440-75umMED HDR feature not supported
acA2500-14gc HDR feature not supported
acA2500-14gm HDR feature not supported
acA2500-14uc HDR feature not supported
acA2500-14um HDR feature not supported
acA2500-20gc HDR feature not supported
acA2500-20gcMED HDR feature not supported
acA2500-20gm HDR feature not supported
acA2500-20gmMED HDR feature not supported
acA2500-60uc HDR feature not supported
acA2500-60um HDR feature not supported
acA3088-16gc HDR feature not supported
acA3088-16gm HDR feature not supported
acA3088-57uc HDR feature not supported
acA3088-57ucMED HDR feature not supported
acA3088-57um HDR feature not supported
acA3088-57umMED HDR feature not supported
acA3800-10gc HDR feature not supported
acA3800-10gm HDR feature not supported
acA3800-14uc HDR feature not supported
acA3800-14um HDR feature not supported
acA4024-8gc HDR feature not supported
acA4024-8gm HDR feature not supported
acA4024-29uc HDR feature not supported
acA4024-29um HDR feature not supported
acA4096-11gc HDR feature not supported
acA4096-11gm HDR feature not supported
acA4096-30uc HDR feature not supported
acA4096-30ucMED HDR feature not supported
acA4096-30um HDR feature not supported
acA4096-30umMED HDR feature not supported
acA4096-40uc HDR feature not supported
acA4096-40ucMED HDR feature not supported
acA4096-40um HDR feature not supported
acA4096-40umMED HDR feature not supported
acA4112-8gc HDR feature not supported
acA4112-8gm HDR feature not supported
acA4112-20uc HDR feature not supported
acA4112-20ucMED HDR feature not supported
acA4112-20um HDR feature not supported
acA4112-20umMED HDR feature not supported
acA4112-30uc HDR feature not supported
acA4112-30ucMED HDR feature not supported
acA4112-30um HDR feature not supported
acA4112-30umMED HDR feature not supported
acA5472-5gc HDR feature not supported
acA5472-5gm HDR feature not supported
acA5472-17uc HDR feature not supported
acA5472-17ucMED HDR feature not supported
acA5472-17um HDR feature not supported
acA5472-17umMED HDR feature not supported
boA1936-400cc HDR feature not supported
boA1936-400cm HDR feature not supported
boA2448-250cc HDR feature not supported
boA2448-250cm HDR feature not supported
boA2832-190cc HDR feature not supported
boA2832-190cm HDR feature not supported
boA4096-93cc HDR feature not supported
boA4096-93cm HDR feature not supported
boA4096-180cc HDR feature not supported
boA4096-180cm HDR feature not supported
boA4112-68cc HDR feature not supported
boA4112-68cm HDR feature not supported
boA4500-45cc HDR feature not supported
boA4500-45cm HDR feature not supported
boA4504-100cc HDR feature not supported
boA4504-100cm HDR feature not supported
boA5120-150cc HDR feature not supported
boA5120-150cm HDR feature not supported
boA5120-230cc HDR feature not supported
boA5120-230cm HDR feature not supported
boA5320-150cc HDR feature not supported
boA5320-150cm HDR feature not supported
boA5328-100cc HDR feature not supported
boA5328-100cm HDR feature not supported
boA6500-36cc HDR feature not supported
boA6500-36cm HDR feature not supported
boA8100-16cc HDR feature not supported
boA8100-16cm HDR feature not supported
boA9344-30cc HDR feature not supported
boA9344-30cm HDR feature not supported
boA9344-70cc HDR feature not supported
boA9344-70cm HDR feature not supported
boA13440-17cm HDR feature not supported
daA720-520uc HDR feature not supported
daA720-520um HDR feature not supported
daA1280-54uc HDR feature not supported
daA1280-54um HDR feature not supported
daA1440-220uc HDR feature not supported
daA1440-220um HDR feature not supported
daA1600-60uc HDR feature not supported
daA1600-60um HDR feature not supported
daA1920-15um HDR feature not supported
daA1920-30uc HDR feature not supported
daA1920-30um HDR feature not supported
daA1920-160uc HDR feature not supported
daA1920-160um HDR feature not supported
daA2448-70uc HDR feature not supported
daA2448-70um HDR feature not supported
daA2500-14uc HDR feature not supported
daA2500-14um HDR feature not supported
daA3840-45uc HDR feature not supported
daA3840-45um HDR feature not supported
dmA720-290gc HDR feature not supported
dmA720-290gm HDR feature not supported
dmA1440-73gc HDR feature not supported
dmA1440-73gm HDR feature not supported
dmA1920-51gc HDR feature not supported
dmA1920-51gm HDR feature not supported
dmA2048-37gc HDR feature not supported
dmA2048-37gm Quad HDR
dmA2448-23gc HDR feature not supported
dmA2448-23gm HDR feature not supported
dmA2840-14gc HDR feature not supported
dmA2840-14gm HDR feature not supported
dmA3536-9gc HDR feature not supported
dmA3536-9gm HDR feature not supported
dmA4096-9gc HDR feature not supported
dmA4096-9gm HDR feature not supported
puA1280-54uc HDR feature not supported
puA1280-54um HDR feature not supported
puA1600-60uc HDR feature not supported
puA1600-60um HDR feature not supported
puA1920-30uc HDR feature not supported
puA1920-30um HDR feature not supported
puA2500-14uc HDR feature not supported
puA2500-14um HDR feature not supported
r2L2048-29gc HDR feature not supported
r2L2048-58gm HDR feature not supported
r2L2048-62cc HDR feature not supported
r2L2048-62g5c HDR feature not supported
r2L2048-172cm HDR feature not supported
r2L2048-172g5m HDR feature not supported
r2L4096-14gc HDR feature not supported
r2L4096-29gm HDR feature not supported
r2L4096-42cc HDR feature not supported
r2L4096-42g5c HDR feature not supported
r2L4096-84cm HDR feature not supported
r2L4096-84g5m HDR feature not supported
r2L8192-200cm HDR feature not supported
r2L16384-120cm HDR feature not supported

Sample Code#

// Set the exposure time mode to Individual
camera.ExposureTimeMode.SetValue(ExposureTimeMode_Individual);
// Select stage 1
camera.ExposureTimeSelector.SetValue(ExposureTimeSelector_Stage1);
// Set the exposure time to 1000 microseconds
camera.ExposureTime.SetValue(1000.0);
// Select stage 2
camera.ExposureTimeSelector.SetValue(ExposureTimeSelector_Stage2);
// Set the exposure time to 1000000 microseconds
camera.ExposureTime.SetValue(1000000.0);
INodeMap& nodemap = camera.GetNodeMap();
// Set the exposure time mode to Individual
CEnumParameter(nodemap, "ExposureTimeMode").SetValue("Individual");
// Select stage 1
CEnumParameter(nodemap, "ExposureTimeSelector").SetValue("Stage1");
// Set the exposure time to 1000 microseconds
CFloatParameter(nodemap, "ExposureTime").SetValue(1000.0);
// Select stage 2
CEnumParameter(nodemap, "ExposureTimeSelector").SetValue("Stage2");
// Set the exposure time to 1000000 microseconds
CFloatParameter(nodemap, "ExposureTime").SetValue(1000000.0);
// Set the exposure time mode to Individual
camera.Parameters[PLCamera.ExposureTimeMode].SetValue(PLCamera.ExposureTimeMode.Individual);
// Select stage 1
camera.Parameters[PLCamera.ExposureTimeSelector].SetValue(PLCamera.ExposureTimeSelector.Stage1);
// Set the exposure time to 1000 microseconds
camera.Parameters[PLCamera.ExposureTime].SetValue(1000.0);
// Select stage 2
camera.Parameters[PLCamera.ExposureTimeSelector].SetValue(PLCamera.ExposureTimeSelector.Stage2);
// Set the exposure time to 1000000 microseconds
camera.Parameters[PLCamera.ExposureTime].SetValue(1000000.0);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Set the exposure time mode to Individual */
errRes = PylonDeviceFeatureFromString(hdev, "ExposureTimeMode", "Individual");
CHECK(errRes);
/* Select stage 1 */
errRes = PylonDeviceFeatureFromString(hdev, "ExposureTimeSelector", "Stage1");
CHECK(errRes);
/* Set the exposure time to 1000 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "ExposureTime", 1000.0);
CHECK(errRes);
/* Select stage 2 */
errRes = PylonDeviceFeatureFromString(hdev, "ExposureTimeSelector", "Stage2");
CHECK(errRes);
/* Set the exposure time to 1000000 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "ExposureTime", 1000000.0);
CHECK(errRes);
# Set the exposure time mode to Individual
camera.ExposureTimeMode.Value = "Individual"
# Select stage 1
camera.ExposureTimeSelector.Value = "Stage1"
# Set the exposure time to 1000 microseconds
camera.ExposureTime.Value = 1000.0
# Select stage 2
camera.ExposureTimeSelector.Value = "Stage2"
# Set the exposure time to 1000000 microseconds
camera.ExposureTime.Value = 1000000.0

You can also use the pylon Viewer to easily set the parameters.