Skip to content

Basler Vision Connector Messaging: Loading the UserSet Configuration#

With the GenICam protocol you can store parameter sets on the camera, and with the Basler Vision Connector you can save, load, and define the default user set to be used on camera restart.

To upload a configured UserSet on the camera, you can send the LoadUserSet message.

JSON Payload#

Field Optional Type Description
TransactionID Yes String Transaction identification
Action No String Method called. Fixed value: LoadUserSet
DeviceID No String Device identification
UserSet No String/Integer (64-bit signed) {Value} or {IntValue} of the User Set Object as defined in Retrieving Available User Sets
{
  "TransactionID": "23423423563456",
  "Action": "LoadUserSet",
  "DeviceID": "548451887",
  "UserSet": "UserSet2"
}

Response Object#

Field Optional Type Description
TransactionID Yes String Transaction identification
ReturnCode No Integer (32-bit unsigned) Message code following Message Codes
Message Yes String Response message
{
  "TransactionID": "1232116",
  "ReturnCode": 0,
  "Message": "User set loaded."
}