Basler_ImageFormatConverterParams#
Classes#
Name | |
---|---|
class | Basler_ImageFormatConverterParams::CImageFormatConverterParams_Params A parameter class containing all parameters as members that are available for Image Format Converter. |
class | Basler_ImageFormatConverterParams::CImageFormatConverterParams_Params_v8_0_0 A parameter class containing all parameters as members that are available for Image Format Converter. |
Types#
Name | |
---|---|
enum | InconvertibleEdgeHandlingEnums { InconvertibleEdgeHandling_Clip, InconvertibleEdgeHandling_Extend, InconvertibleEdgeHandling_SetZero} Valid values for InconvertibleEdgeHandling. |
enum | MonoConversionMethodEnums { MonoConversionMethod_Gamma, MonoConversionMethod_Truncate} Valid values for MonoConversionMethod. |
enum | OutputBitAlignmentEnums { OutputBitAlignment_LsbAligned, OutputBitAlignment_MsbAligned} Valid values for OutputBitAlignment. |
enum | OutputOrientationEnums { OutputOrientation_BottomUp, OutputOrientation_TopDown, OutputOrientation_Unchanged} Valid values for OutputOrientation. |
Types Documentation#
enum InconvertibleEdgeHandlingEnums#
Enumerator | Value | Description |
---|---|---|
InconvertibleEdgeHandling_Clip | Rows and columns that can't be converted are removed from the output image - Applies to: ImageFormatConverter. | |
InconvertibleEdgeHandling_Extend | Rows and columns that can't be converted are filled by extrapolating image data from neighboring rows and columns - Applies to: ImageFormatConverter. | |
InconvertibleEdgeHandling_SetZero | Rows and columns that can't be converted are set to zero - Applies to: ImageFormatConverter. |
enum MonoConversionMethodEnums#
Enumerator | Value | Description |
---|---|---|
MonoConversionMethod_Gamma | When converting images, Gamma conversion is used - Applies to: ImageFormatConverter. | |
MonoConversionMethod_Truncate | When converting images, image data is shifted - Applies to: ImageFormatConverter. |
Valid values for MonoConversionMethod.
enum OutputBitAlignmentEnums#
Enumerator | Value | Description |
---|---|---|
OutputBitAlignment_LsbAligned | Image data is aligned with the least significant bit - Applies to: ImageFormatConverter. | |
OutputBitAlignment_MsbAligned | The data is aligned at the most significant bit - Applies to: ImageFormatConverter. |
Valid values for OutputBitAlignment.
enum OutputOrientationEnums#
Enumerator | Value | Description |
---|---|---|
OutputOrientation_BottomUp | The last row of the image is located at the start of the image buffer - Applies to: ImageFormatConverter. | |
OutputOrientation_TopDown | The first row of the image is located at the start of the image buffer - Applies to: ImageFormatConverter. | |
OutputOrientation_Unchanged | The orientation of the image remains the same - Applies to: ImageFormatConverter. |
Valid values for OutputOrientation.