PLCamera.CounterResetSourceEnum Class#
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
Visibility: Beginner
Selected by: CounterSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.CounterResetSourceEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.CounterResetSourceEnum | Initializes a new instance of the PLCamera.CounterResetSourceEnum class |
Properties#
Name | Description | |
---|---|---|
AcquisitionActive | The selected counter can be reset by an Acquisition Active signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Action1 | The selected counter can be reset by an action command that is defined by action signal 1. Applies to: ace 2 GigE | |
Action2 | The selected counter can be reset by an action command that is defined by action signal 2. Applies to: ace 2 GigE | |
CC1 | The selected counter can be reset by a CC1 signal. Applies to: CameraLink and GigE | |
CC2 | The selected counter can be reset by a CC2 signal. Applies to: CameraLink and GigE | |
CC3 | The selected counter can be reset by a CC3 signal. Applies to: CameraLink and GigE | |
CC4 | The selected counter can be reset by a CC4 signal. Applies to: CameraLink and GigE | |
Counter1Active | The selected counter can be reset by a Counter 1 Active signal. By default, a Counter 1 Active signal is generated whenever counter 1 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter1End | The selected counter can be reset by a Counter End 1 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter1Start | The selected counter can be reset by a Counter 1 Start signal. A Counter 1 Start signal is generated whenever counter 1 is started. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter2Active | The selected counter can be reset by a Counter 2 Active signal. By default, a Counter 2 Active signal is generated whenever counter 2 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter2End | The selected counter can be reset by a Counter End 2 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter2Start | The selected counter can be reset by a Counter 2 Start signal. A Counter 2 Start signal is generated whenever counter 2 is started. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter3End | The selected counter can be reset by a counter end 3 signal. Applies to: ace USB | |
Counter4End | The selected counter can be reset by a counter end 4 signal. Applies to: ace USB | |
CxpTrigger0 | The selected counter can be reset by a CXP Trigger 0 signal. Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP | |
CxpTrigger1 | The selected counter can be reset by a CXP Trigger 1 signal. Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP | |
ExposureActive | The selected counter can be reset by an Exposure Active signal. By default, an Exposure Active signal is generated whenever exposure is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
ExposureStart | The selected counter can be reset by an Exposure Start signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
ExposureTriggerWait | The selected counter can be reset by an Exposure Trigger Wait signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
FlashWindow | The selected counter can be reset by a Flash Window signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress and dart USB | |
FrameBurstActive | The selected counter can be reset by a Frame Burst Active signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
FrameBurstTriggerWait | The selected counter can be reset by a Frame Burst Trigger Wait signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
FrameTriggerWait | The selected counter can be reset by a Frame Trigger Wait signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line1 | The selected counter can be reset by a signal applied to Line 1. Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line2 | The selected counter can be reset by a signal applied to Line 2. Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line3 | The selected counter can be reset by a signal applied to Line 3. Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line4 | The selected counter can be reset by a signal applied to Line 4. Applies to: CameraLink, GigE, ace USB, dart 2 USB and dart USB | |
Line5 | The selected counter can be reset by a signal applied to Line 5. Applies to: CameraLink and GigE | |
Line6 | The selected counter can be reset by a signal applied to Line 6. Applies to: CameraLink and GigE | |
Line7 | The selected counter can be reset by a signal applied to Line 7. Applies to: CameraLink and GigE | |
Line8 | The selected counter can be reset by a signal applied to Line 8. Applies to: CameraLink and GigE | |
Name | The full name of CounterResetSource (Overrides ParameterListEnum.Name.) | |
Off | The counter reset is disabled. Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
PeriodicSignal1 | The selected counter can be reset by a Periodic Signal 1 signal. Applies to: ace 2 GigE | |
Software | The selected counter can be reset by a software command. Applies to: CameraLink, GigE and ace USB | |
SoftwareSignal1 | The selected counter can be reset by a Software Signal 1 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
SoftwareSignal2 | The selected counter can be reset by a Software Signal 2 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
SoftwareSignal3 | The selected counter can be reset by a Software Signal 3 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Timer1Active | The selected counter can be reset by a Timer 1 Active signal. By default, a Timer 1 Active signal is generated whenever timer 1 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Timer1End | The selected counter can be reset by a Timer 1 End signal. A Timer 1 End signal is generated whenever timer 1 has elapsed. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Timer2Active | The selected counter can be reset by a Timer 2 Active signal. By default, a Timer 2 Active signal is generated whenever timer 2 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Timer2End | The selected counter can be reset by a Timer 2 End signal. A Timer 2 End signal is generated whenever timer 2 has elapsed. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
VInput1 | This enumeration value selects VInput1 as the source for counter reset. Applies to: CameraLink and GigE | |
VInput2 | This enumeration value selects VInput2 as the source for counter reset. Applies to: CameraLink and GigE | |
VInput3 | This enumeration value selects VInput3 as the source for counter reset. Applies to: CameraLink and GigE | |
VInput4 | This enumeration value selects VInput4 as the source for counter reset. Applies to: CameraLink and GigE | |
VInputDecActive | This enumeration value selects Virtual Input Decoder Active as the source for counter reset. Applies to: CameraLink and GigE |
Methods#
Name | Description | |
---|---|---|
ToString | The full name of CounterResetSource (Overrides Object.ToString()()()().) |
PLCamera.CounterResetSourceEnum.ToString Method#
The full name of CounterResetSource
Return Value#
Type: String
Returns the full name of CounterResetSource
PLCamera.CounterResetSourceEnum Constructor#
Initializes a new instance of the PLCamera.CounterResetSourceEnum class
PLCamera.CounterResetSourceEnum.AcquisitionActive Property#
The selected counter can be reset by an Acquisition Active signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Action1 Property#
The selected counter can be reset by an action command that is defined by action signal 1.
Applies to: ace 2 GigE
PLCamera.CounterResetSourceEnum.Action2 Property#
The selected counter can be reset by an action command that is defined by action signal 2.
Applies to: ace 2 GigE
PLCamera.CounterResetSourceEnum.CC1 Property#
The selected counter can be reset by a CC1 signal.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.CC2 Property#
The selected counter can be reset by a CC2 signal.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.CC3 Property#
The selected counter can be reset by a CC3 signal.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.CC4 Property#
The selected counter can be reset by a CC4 signal.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.Counter1Active Property#
The selected counter can be reset by a Counter 1 Active signal. By default, a Counter 1 Active signal is generated whenever counter 1 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Counter1End Property#
The selected counter can be reset by a Counter End 1 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Counter1Start Property#
The selected counter can be reset by a Counter 1 Start signal. A Counter 1 Start signal is generated whenever counter 1 is started.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Counter2Active Property#
The selected counter can be reset by a Counter 2 Active signal. By default, a Counter 2 Active signal is generated whenever counter 2 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Counter2End Property#
The selected counter can be reset by a Counter End 2 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Counter2Start Property#
The selected counter can be reset by a Counter 2 Start signal. A Counter 2 Start signal is generated whenever counter 2 is started.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Counter3End Property#
The selected counter can be reset by a counter end 3 signal.
Applies to: ace USB
PLCamera.CounterResetSourceEnum.Counter4End Property#
The selected counter can be reset by a counter end 4 signal.
Applies to: ace USB
PLCamera.CounterResetSourceEnum.CxpTrigger0 Property#
The selected counter can be reset by a CXP Trigger 0 signal.
Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP
PLCamera.CounterResetSourceEnum.CxpTrigger1 Property#
The selected counter can be reset by a CXP Trigger 1 signal.
Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP
PLCamera.CounterResetSourceEnum.ExposureActive Property#
The selected counter can be reset by an Exposure Active signal. By default, an Exposure Active signal is generated whenever exposure is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.ExposureStart Property#
The selected counter can be reset by an Exposure Start signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.ExposureTriggerWait Property#
The selected counter can be reset by an Exposure Trigger Wait signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.FlashWindow Property#
The selected counter can be reset by a Flash Window signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress and dart USB
PLCamera.CounterResetSourceEnum.FrameBurstActive Property#
The selected counter can be reset by a Frame Burst Active signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.FrameBurstTriggerWait Property#
The selected counter can be reset by a Frame Burst Trigger Wait signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.FrameTriggerWait Property#
The selected counter can be reset by a Frame Trigger Wait signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Line1 Property#
The selected counter can be reset by a signal applied to Line 1.
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Line2 Property#
The selected counter can be reset by a signal applied to Line 2.
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Line3 Property#
The selected counter can be reset by a signal applied to Line 3.
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Line4 Property#
The selected counter can be reset by a signal applied to Line 4.
Applies to: CameraLink, GigE, ace USB, dart 2 USB and dart USB
PLCamera.CounterResetSourceEnum.Line5 Property#
The selected counter can be reset by a signal applied to Line 5.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.Line6 Property#
The selected counter can be reset by a signal applied to Line 6.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.Line7 Property#
The selected counter can be reset by a signal applied to Line 7.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.Line8 Property#
The selected counter can be reset by a signal applied to Line 8.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.Name Property#
The full name of CounterResetSource
PLCamera.CounterResetSourceEnum.Off Property#
The counter reset is disabled.
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.PeriodicSignal1 Property#
The selected counter can be reset by a Periodic Signal 1 signal.
Applies to: ace 2 GigE
PLCamera.CounterResetSourceEnum.Software Property#
The selected counter can be reset by a software command.
Applies to: CameraLink, GigE and ace USB
PLCamera.CounterResetSourceEnum.SoftwareSignal1 Property#
The selected counter can be reset by a Software Signal 1 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.SoftwareSignal2 Property#
The selected counter can be reset by a Software Signal 2 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.SoftwareSignal3 Property#
The selected counter can be reset by a Software Signal 3 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Timer1Active Property#
The selected counter can be reset by a Timer 1 Active signal. By default, a Timer 1 Active signal is generated whenever timer 1 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Timer1End Property#
The selected counter can be reset by a Timer 1 End signal. A Timer 1 End signal is generated whenever timer 1 has elapsed.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Timer2Active Property#
The selected counter can be reset by a Timer 2 Active signal. By default, a Timer 2 Active signal is generated whenever timer 2 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.Timer2End Property#
The selected counter can be reset by a Timer 2 End signal. A Timer 2 End signal is generated whenever timer 2 has elapsed.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterResetSourceEnum.VInput1 Property#
This enumeration value selects VInput1 as the source for counter reset.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.VInput2 Property#
This enumeration value selects VInput2 as the source for counter reset.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.VInput3 Property#
This enumeration value selects VInput3 as the source for counter reset.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.VInput4 Property#
This enumeration value selects VInput4 as the source for counter reset.
Applies to: CameraLink and GigE
PLCamera.CounterResetSourceEnum.VInputDecActive Property#
This enumeration value selects Virtual Input Decoder Active as the source for counter reset.
Applies to: CameraLink and GigE