PLCamera.LineSelectorEnum Class#
Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB and racer 2 CXP
Visibility: Beginner
Selecting Parameters: BslInputFilterTime, BslInputHoldOffTime, BslLineConnection, BslLineOverloadStatus, BslLineTermination, LineDebouncerTime, LineDebouncerTimeAbs, LineFormat, LineInverter, LineLogic, LineMinimumOutputPulseWidth, LineMode, LineOverloadReset, LineOverloadStatus, LineSource, LineStatus, LineTermination, MinOutPulseWidthAbs
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.LineSelectorEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.LineSelectorEnum | Initializes a new instance of the PLCamera.LineSelectorEnum class |
Properties#
Name | Description | |
---|---|---|
CC1 | CC1 can be configured. Applies to: CameraLink | |
CC2 | CC2 can be configured. Applies to: CameraLink | |
CC3 | CC3 can be configured. Applies to: CameraLink | |
CC4 | CC4 can be configured. Applies to: CameraLink | |
ClSpare | The CL Spare line can be configured. Applies to: CameraLink | |
In1 | This enumeration value selects input line 1 for configuration. Applies to: CameraLink | |
In2 | This enumeration value selects input line 2 for configuration. Applies to: CameraLink | |
In3 | This enumeration value selects input line 3 for configuration. Applies to: CameraLink | |
In4 | This enumeration value selects input line 4 for configuration. Applies to: CameraLink | |
Line1 | Line 1 can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line2 | Line 2 can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line3 | Line 3 can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line4 | Line 4 can be configured. Applies to: CameraLink, GigE, ace USB, dart 2 USB and dart USB | |
Line5 | This enumeration value selects line 5 for configuration. Applies to: CameraLink | |
Line6 | This enumeration value selects line 6 for configuration. Applies to: CameraLink | |
Line7 | This enumeration value selects line 7 for configuration. Applies to: CameraLink | |
Line8 | This enumeration value selects line 8 for configuration. Applies to: CameraLink | |
Name | The full name of LineSelector (Overrides ParameterListEnum.Name.) | |
Out1 | Output Line 1 can be configured. Applies to: CameraLink and GigE | |
Out2 | Output Line 2 can be configured. Applies to: CameraLink and GigE | |
Out3 | Output Line 3 can be configured. Applies to: CameraLink and GigE | |
Out4 | Output Line 4 can be configured. Applies to: CameraLink and GigE |
Methods#
Name | Description | |
---|---|---|
ToString | The full name of LineSelector (Overrides Object.ToString()()()().) |
PLCamera.LineSelectorEnum.ToString Method#
The full name of LineSelector
Return Value#
Type: String
Returns the full name of LineSelector
PLCamera.LineSelectorEnum Constructor#
Initializes a new instance of the PLCamera.LineSelectorEnum class
PLCamera.LineSelectorEnum.CC1 Property#
CC1 can be configured.
Applies to: CameraLink
PLCamera.LineSelectorEnum.CC2 Property#
CC2 can be configured.
Applies to: CameraLink
PLCamera.LineSelectorEnum.CC3 Property#
CC3 can be configured.
Applies to: CameraLink
PLCamera.LineSelectorEnum.CC4 Property#
CC4 can be configured.
Applies to: CameraLink
PLCamera.LineSelectorEnum.ClSpare Property#
The CL Spare line can be configured.
Applies to: CameraLink
PLCamera.LineSelectorEnum.In1 Property#
This enumeration value selects input line 1 for configuration.
Applies to: CameraLink
PLCamera.LineSelectorEnum.In2 Property#
This enumeration value selects input line 2 for configuration.
Applies to: CameraLink
PLCamera.LineSelectorEnum.In3 Property#
This enumeration value selects input line 3 for configuration.
Applies to: CameraLink
PLCamera.LineSelectorEnum.In4 Property#
This enumeration value selects input line 4 for configuration.
Applies to: CameraLink
PLCamera.LineSelectorEnum.Line1 Property#
Line 1 can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.LineSelectorEnum.Line2 Property#
Line 2 can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.LineSelectorEnum.Line3 Property#
Line 3 can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.LineSelectorEnum.Line4 Property#
Line 4 can be configured.
Applies to: CameraLink, GigE, ace USB, dart 2 USB and dart USB
PLCamera.LineSelectorEnum.Line5 Property#
This enumeration value selects line 5 for configuration.
Applies to: CameraLink
PLCamera.LineSelectorEnum.Line6 Property#
This enumeration value selects line 6 for configuration.
Applies to: CameraLink
PLCamera.LineSelectorEnum.Line7 Property#
This enumeration value selects line 7 for configuration.
Applies to: CameraLink
PLCamera.LineSelectorEnum.Line8 Property#
This enumeration value selects line 8 for configuration.
Applies to: CameraLink
PLCamera.LineSelectorEnum.Name Property#
The full name of LineSelector
PLCamera.LineSelectorEnum.Out1 Property#
Output Line 1 can be configured.
Applies to: CameraLink and GigE
PLCamera.LineSelectorEnum.Out2 Property#
Output Line 2 can be configured.
Applies to: CameraLink and GigE
PLCamera.LineSelectorEnum.Out3 Property#
Output Line 3 can be configured.
Applies to: CameraLink and GigE
PLCamera.LineSelectorEnum.Out4 Property#
Output Line 4 can be configured.
Applies to: CameraLink and GigE