PLCamera.CounterTriggerSourceEnum Class#
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
Visibility: Expert
Selected by: CounterSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.CounterTriggerSourceEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.CounterTriggerSourceEnum | Initializes a new instance of the PLCamera.CounterTriggerSourceEnum class |
Properties#
Name | Description | |
---|---|---|
AcquisitionActive | The selected counter can be started by an Acquisition Active signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Action1 | The selected counter can be started by an action command that is defined by action signal 1. Applies to: ace 2 GigE | |
Action2 | The selected counter can be started by an action command that is defined by action signal 2. Applies to: ace 2 GigE | |
Counter1Active | The selected counter can be started by a Counter 1 Active signal. By default, a Counter 1 Active signal is generated whenever counter 1 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter1End | The selected counter can be started by a Counter 1 End signal. A Counter 1 End signal is generated whenever counter 1 is stopped, reset, or when it has reached its maximum value. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter1Start | The selected counter can be started by a Counter 1 Start signal. A Counter 1 Start signal is generated whenever counter 1 is started. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter2Active | The selected counter can be started by a Counter 2 Active signal. By default, a Counter 2 Active signal is generated whenever counter 2 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter2End | The selected counter can be started by a Counter 2 End signal. A Counter 2 End signal is generated whenever counter 2 is stopped, reset, or when it has reached its maximum value. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Counter2Start | The selected counter can be started by a Counter 2 Start signal. A Counter 2 Start signal is generated whenever counter 2 is started. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
CxpTrigger0 | The selected counter can be started by a CXP Trigger 0 signal. Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP | |
CxpTrigger1 | The selected counter can be started by a CXP Trigger 1 signal. Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP | |
ExposureActive | The selected counter can be started by an Exposure Active signal. By default, an Exposure Active signal is generated whenever exposure is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
ExposureStart | The selected counter can be started by an Exposure Start signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
ExposureTriggerWait | The selected counter can be started by an Exposure Trigger Wait signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
FlashWindow | The selected counter can be started by a Flash Window signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress and dart USB | |
FrameBurstActive | The selected counter can be started by a Frame Burst Active signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
FrameBurstTriggerWait | The selected counter can be started by a Frame Burst Trigger Wait signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
FrameTriggerWait | The selected counter can be started by a Frame Trigger Wait signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line1 | The selected counter can be started by a Line 1 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line2 | The selected counter can be started by a Line 2 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line3 | The selected counter can be started by a Line 3 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Line4 | The selected counter can be started by a Line 4 signal. Applies to: dart 2 USB and dart USB | |
Name | The full name of CounterTriggerSource (Overrides ParameterListEnum.Name.) | |
Off | The selected counter is disabled and can't be started. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
PeriodicSignal1 | The selected counter can be started by a Periodic Signal 1 signal. Applies to: ace 2 GigE | |
SoftwareSignal1 | The selected counter can be started by a Software Signal 1 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
SoftwareSignal2 | The selected counter can be started by a Software Signal 2 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
SoftwareSignal3 | The selected counter can be started by a Software Signal 3 signal. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Timer1Active | The selected counter can be started by a Timer 1 Active signal. By default, a Timer 1 Active signal is generated whenever timer 1 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Timer1End | The selected counter can be started by a Timer 1 End signal. A Timer 1 End signal is generated whenever timer 1 has elapsed. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Timer2Active | The selected counter can be started by a Timer 2 Active signal. By default, a Timer 2 Active signal is generated whenever timer 2 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP | |
Timer2End | The selected counter can be started by a Timer 2 End signal. A Timer 2 End signal is generated whenever timer 2 has elapsed. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP |
Methods#
Name | Description | |
---|---|---|
ToString | The full name of CounterTriggerSource (Overrides Object.ToString()()()().) |
PLCamera.CounterTriggerSourceEnum.ToString Method#
The full name of CounterTriggerSource
Return Value#
Type: String
Returns the full name of CounterTriggerSource
PLCamera.CounterTriggerSourceEnum Constructor#
Initializes a new instance of the PLCamera.CounterTriggerSourceEnum class
PLCamera.CounterTriggerSourceEnum.AcquisitionActive Property#
The selected counter can be started by an Acquisition Active signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Action1 Property#
The selected counter can be started by an action command that is defined by action signal 1.
Applies to: ace 2 GigE
PLCamera.CounterTriggerSourceEnum.Action2 Property#
The selected counter can be started by an action command that is defined by action signal 2.
Applies to: ace 2 GigE
PLCamera.CounterTriggerSourceEnum.Counter1Active Property#
The selected counter can be started by a Counter 1 Active signal. By default, a Counter 1 Active signal is generated whenever counter 1 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Counter1End Property#
The selected counter can be started by a Counter 1 End signal. A Counter 1 End signal is generated whenever counter 1 is stopped, reset, or when it has reached its maximum value.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Counter1Start Property#
The selected counter can be started by a Counter 1 Start signal. A Counter 1 Start signal is generated whenever counter 1 is started.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Counter2Active Property#
The selected counter can be started by a Counter 2 Active signal. By default, a Counter 2 Active signal is generated whenever counter 2 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Counter2End Property#
The selected counter can be started by a Counter 2 End signal. A Counter 2 End signal is generated whenever counter 2 is stopped, reset, or when it has reached its maximum value.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Counter2Start Property#
The selected counter can be started by a Counter 2 Start signal. A Counter 2 Start signal is generated whenever counter 2 is started.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.CxpTrigger0 Property#
The selected counter can be started by a CXP Trigger 0 signal.
Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.CxpTrigger1 Property#
The selected counter can be started by a CXP Trigger 1 signal.
Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.ExposureActive Property#
The selected counter can be started by an Exposure Active signal. By default, an Exposure Active signal is generated whenever exposure is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.ExposureStart Property#
The selected counter can be started by an Exposure Start signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.ExposureTriggerWait Property#
The selected counter can be started by an Exposure Trigger Wait signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.FlashWindow Property#
The selected counter can be started by a Flash Window signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress and dart USB
PLCamera.CounterTriggerSourceEnum.FrameBurstActive Property#
The selected counter can be started by a Frame Burst Active signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.FrameBurstTriggerWait Property#
The selected counter can be started by a Frame Burst Trigger Wait signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.FrameTriggerWait Property#
The selected counter can be started by a Frame Trigger Wait signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Line1 Property#
The selected counter can be started by a Line 1 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Line2 Property#
The selected counter can be started by a Line 2 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Line3 Property#
The selected counter can be started by a Line 3 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Line4 Property#
The selected counter can be started by a Line 4 signal.
Applies to: dart 2 USB and dart USB
PLCamera.CounterTriggerSourceEnum.Name Property#
The full name of CounterTriggerSource
PLCamera.CounterTriggerSourceEnum.Off Property#
The selected counter is disabled and can't be started.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.PeriodicSignal1 Property#
The selected counter can be started by a Periodic Signal 1 signal.
Applies to: ace 2 GigE
PLCamera.CounterTriggerSourceEnum.SoftwareSignal1 Property#
The selected counter can be started by a Software Signal 1 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.SoftwareSignal2 Property#
The selected counter can be started by a Software Signal 2 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.SoftwareSignal3 Property#
The selected counter can be started by a Software Signal 3 signal.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Timer1Active Property#
The selected counter can be started by a Timer 1 Active signal. By default, a Timer 1 Active signal is generated whenever timer 1 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Timer1End Property#
The selected counter can be started by a Timer 1 End signal. A Timer 1 End signal is generated whenever timer 1 has elapsed.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Timer2Active Property#
The selected counter can be started by a Timer 2 Active signal. By default, a Timer 2 Active signal is generated whenever timer 2 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP
PLCamera.CounterTriggerSourceEnum.Timer2End Property#
The selected counter can be started by a Timer 2 End signal. A Timer 2 End signal is generated whenever timer 2 has elapsed.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP