Skip to content

PLCamera.BinningVerticalModeEnum Class#

Sets the binning mode for vertical binning.

Applies to: CamEmu, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP

Visibility: Expert

Selected by: BinningSelector

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BinningVerticalModeEnum

Constructors#

 NameDescription
Public methodPLCamera.BinningVerticalModeEnum Initializes a new instance of the PLCamera.BinningVerticalModeEnum class
 

Properties#

 NameDescription
Public propertyAverage

The values of the binned pixels are averaged. This increases the signal-to-noise ratio without affecting the camera's response to light.

Applies to: CamEmu, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP

Public propertyName The full name of BinningVerticalMode (Overrides ParameterListEnum.Name.)
Public propertySum

The values of the binned pixels are summed. This increases the camera's response to light and the signal-to-noise ratio.

Applies to: CamEmu, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP

 

Methods#

 NameDescription
Public methodToString The full name of BinningVerticalMode (Overrides Object.ToString()()()().)
 

PLCamera.BinningVerticalModeEnum.ToString Method#

The full name of BinningVerticalMode

Return Value#

Type: String
Returns the full name of BinningVerticalMode

PLCamera.BinningVerticalModeEnum Constructor#

Initializes a new instance of the PLCamera.BinningVerticalModeEnum class

PLCamera.BinningVerticalModeEnum.Average Property#

The values of the binned pixels are averaged. This increases the signal-to-noise ratio without affecting the camera's response to light.

Applies to: CamEmu, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP

PLCamera.BinningVerticalModeEnum.Name Property#

The full name of BinningVerticalMode

PLCamera.BinningVerticalModeEnum.Sum Property#

The values of the binned pixels are summed. This increases the camera's response to light and the signal-to-noise ratio.

Applies to: CamEmu, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP