Basler Vision Connector#
Info
You can configure different Basler camera models (GigE, USB) with the Basler Vision Connector app. However, the Basler Vision Connector app only supports GigE cameras as the Siemens Industrial Edge devices can currently only deal with GigE cameras, e.g., Basler ace 2.
Required Knowledge#
The Basler Vision Connector and Basler digital cameras for machine vision are designed for use by professionals only, concerned with the following tasks:
- Camera integration and setup
- Everyday camera use
For installing and configuring your Industrial Edge devices and the Basler Vision Connector app, you require the following knowledge:
- Knowledge about MQTT / ZeroMQ protocol communication
- Knowledge working with Docker and Docker container is helpful.
The Basler Vision Connector documentation assumes the skills of electrical engineers, systems engineers, mechatronics engineers, technicians, and information technology engineers. Basler Vision Connector and camera use isn't allowed for persons with insufficient skills or with impairments that prevent them from doing the following tasks:
- Using cameras correctly
- Adhering to the safety instructions
- Fully understanding all relevant camera documentation and other linked documentation
Additional Information#
- For camera and accessory information, see the Camera Documentation or the Accessories Documentation.
- For detailed information about Siemens IE devices and management, see the Siemens Industrial Edge Documentation
Prerequisites#
To install and use the Basler Vision Connector, you need the following tools and hardware:
- A working Internet connection.
- Memory limit:
- Basler Vision Connector Multi Camera Connection app: 2 GB of free memory space on your Edge Device.
- Basler Vision Connector Single Camera Connection app: 1 GB of free memory space on your Edge Device.
The memory limit reserves the maximum memory space needed by the Basler Vision Connector. The actual used memory depends on the number of cameras used, the image sizes and amount of frame buffers used (default is 10 frame buffers per camera). If you have a scenario in your project that requires less memory, e.g., if you have only one camera with a small image size and a small number of frame buffers, you can disable the memory limit check as described in the Siemens Industrial Edge Device documentation.
- To connect your GigE camera, Basler recommends using the BX-59A, or BX-39A Industrial Edge device. See Connecting Cameras.
- If you want to connect more than one GigE camera with the BX-59A or BX-39A IED, Basler recommends to use one of the following network switches:
- Netgear GS110TP, or
- Netgear MS510TXPP for a broader bandwidth.
- For 10GigE cameras, Basler recommends using the BX-59A device with a network interface card (such as the Broadcom NetXtreme 2x 10GbE, LAN-Adapter).
- Access to the Siemens Industrial Edge Hub (provided by Siemens).
Contact Siemens to get your personal access to the hub. - Installed and configured Siemens IEM Instances and all IE devices you require for your use case. For information about installing the IEM instances and IE devices, see the Siemens documentation.
- Installed Basler camera.
For further information about Basler camera installation and configuration:- Go to the Camera Documentation, select the camera model you installed in your factory or search for your camera model via the camera filter (located to the left of the Search field of this documentation).
- When the camera model is selected, the camera and its feature documentation are displayed. Read the safety instructions of your camera model.
- The following Basler Vision Connector applications are available in the Siemens marketplace:
- Basler Vision Connector (Single Camera Connection):
Use this app, if you want to use only one camera. - Basler Vision Connector (Multi Camera Connection):
Use this app, if you want to use several cameras.
- Basler Vision Connector (Single Camera Connection):
Info
Basler recommends to not install a Basler Vision Connector (Single Camera Connection) and Basler Vision Connector (Multi Camera Connection) on the same Edge Device.
- Programming and test tools:
- You can use the Siemens Industrial Edge Flow Creator application (IE Flow Creator).
- The IE Flow Creator uses the flow-based Node-RED development tool.
- Siemens Databus application for testing.
- Siemens Data Flow Monitoring application.