Skip to content

PLCamera.TimerTriggerSourceEnum Class#

Sets the internal camera signal used to trigger the selected timer.

Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Visibility: Beginner

Selected by: TimerSelector

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.TimerTriggerSourceEnum

Constructors#

 NameDescription
Public methodPLCamera.TimerTriggerSourceEnum Initializes a new instance of the PLCamera.TimerTriggerSourceEnum class
 

Properties#

 NameDescription
Public propertyAcquisitionActive

The selected timer can be started by an Acquisition Active signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyAction1

The selected timer can be started by an action signal that is defined by action signal 1.

Applies to: ace 2 GigE

Public propertyAction2

The selected timer can be started by an action signal that is defined by action signal 2.

Applies to: ace 2 GigE

Public propertyCounter1Active

The selected timer can be started by a Counter 1 Active signal. By default, a Counter 1 Active signal is generated whenever timer 1 is started. You can change this behavior using the Counter Event Activation parameter.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyCounter1End

The selected timer can be started by a Counter 1 End signal. A Counter 1 End signal is generated whenever timer 1 is stopped, reset, or when it has reached its maximum value.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyCounter1Start

The selected timer can be started by a Counter 1 Start signal. A Counter 1 Start signal is generated whenever timer 1 is started.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyCounter2Active

The selected timer can be started by a Counter 2 Active signal. By default, a Counter 2 Active signal is generated whenever timer 2 is started. You can change this behavior using the Counter Event Activation parameter.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyCounter2End

The selected timer can be started by a Counter 2 End signal. A Counter 2 End signal is generated whenever timer 2 is stopped, reset, or when it has reached its maximum value.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyCounter2Start

The selected timer can be started by a Counter 2 Start signal. A Counter 2 Start signal is generated whenever timer 2 is started.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyCxpTrigger0

The selected timer can be started by a CXP Trigger 0 signal.

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

Public propertyCxpTrigger1

The selected timer can be started by a CXP Trigger 1 signal.

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

Public propertyExposureActive

The selected timer can be started by an Exposure Active signal. By default, an Exposure Active signal is generated whenever exposure is started. You can change this behavior using the Counter Event Activation parameter.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyExposureStart

The selected timer can be started by an Exposure Start signal.

Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyExposureTriggerWait

The selected timer can be started by an Exposure Trigger Wait signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyFlashWindow

The selected timer can be started by a Flash Window signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress and dart USB

Public propertyFlashWindowStart

Starts with the reception of the flash window start.

Applies to: GigE and ace USB

Public propertyFrameBurstActive

The selected timer can be started by a Frame Burst Active signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyFrameBurstTriggerWait

The selected timer can be started by a Frame Burst Trigger Wait signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyFrameTriggerWait

The selected timer can be started by a Frame Trigger Wait signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyLine1

The selected timer can be started by a Line 1 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyLine2

The selected timer can be started by a Line 2 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyLine3

The selected timer can be started by a Line 3 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyLine4

The selected timer can be started by a Line 4 signal.

Applies to: dart 2 USB and dart USB

Public propertyName The full name of TimerTriggerSource (Overrides ParameterListEnum.Name.)
Public propertyOff

The selected timer is disabled and can't be started.

Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyPeriodicSignal1

The selected timer can be started by a Periodic Signal 1 signal.

Applies to: ace 2 GigE

Public propertySoftwareSignal1

The selected timer can be started by a Software Signal 1 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertySoftwareSignal2

The selected timer can be started by a Software Signal 2 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertySoftwareSignal3

The selected timer can be started by a Software Signal 3 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyTimer1Active

The selected timer can be started by a Timer 1 Active signal. By default, a Timer 1 Active signal is generated whenever timer 1 has been started. You can change this behavior using the Counter Event Activation parameter.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyTimer1End

The selected timer can be started by a Timer 1 End signal. A Timer 1 End signal is generated whenever timer 1 has elapsed.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyTimer2Active

The selected timer can be started by a Timer 2 Active signal. By default, a Timer 2 Active signal is generated whenever timer 2 is started. You can change this behavior using the Counter Event Activation parameter.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

Public propertyTimer2End

The selected timer can be started by a Timer 2 End signal. A Timer 2 End signal is generated whenever timer 2 has elapsed.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

 

Methods#

 NameDescription
Public methodToString The full name of TimerTriggerSource (Overrides Object.ToString()()()().)
 

PLCamera.TimerTriggerSourceEnum.ToString Method#

The full name of TimerTriggerSource

Return Value#

Type: String
Returns the full name of TimerTriggerSource

PLCamera.TimerTriggerSourceEnum Constructor#

Initializes a new instance of the PLCamera.TimerTriggerSourceEnum class

PLCamera.TimerTriggerSourceEnum.AcquisitionActive Property#

The selected timer can be started by an Acquisition Active signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Action1 Property#

The selected timer can be started by an action signal that is defined by action signal 1.

Applies to: ace 2 GigE

PLCamera.TimerTriggerSourceEnum.Action2 Property#

The selected timer can be started by an action signal that is defined by action signal 2.

Applies to: ace 2 GigE

PLCamera.TimerTriggerSourceEnum.Counter1Active Property#

The selected timer can be started by a Counter 1 Active signal. By default, a Counter 1 Active signal is generated whenever timer 1 is started. You can change this behavior using the Counter Event Activation parameter.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Counter1End Property#

The selected timer can be started by a Counter 1 End signal. A Counter 1 End signal is generated whenever timer 1 is stopped, reset, or when it has reached its maximum value.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Counter1Start Property#

The selected timer can be started by a Counter 1 Start signal. A Counter 1 Start signal is generated whenever timer 1 is started.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Counter2Active Property#

The selected timer can be started by a Counter 2 Active signal. By default, a Counter 2 Active signal is generated whenever timer 2 is started. You can change this behavior using the Counter Event Activation parameter.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Counter2End Property#

The selected timer can be started by a Counter 2 End signal. A Counter 2 End signal is generated whenever timer 2 is stopped, reset, or when it has reached its maximum value.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Counter2Start Property#

The selected timer can be started by a Counter 2 Start signal. A Counter 2 Start signal is generated whenever timer 2 is started.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.CxpTrigger0 Property#

The selected timer can be started by a CXP Trigger 0 signal.

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.CxpTrigger1 Property#

The selected timer can be started by a CXP Trigger 1 signal.

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.ExposureActive Property#

The selected timer can be started by an Exposure Active signal. By default, an Exposure Active signal is generated whenever exposure is started. You can change this behavior using the Counter Event Activation parameter.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.ExposureStart Property#

The selected timer can be started by an Exposure Start signal.

Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.ExposureTriggerWait Property#

The selected timer can be started by an Exposure Trigger Wait signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.FlashWindow Property#

The selected timer can be started by a Flash Window signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress and dart USB

PLCamera.TimerTriggerSourceEnum.FlashWindowStart Property#

Starts with the reception of the flash window start.

Applies to: GigE and ace USB

PLCamera.TimerTriggerSourceEnum.FrameBurstActive Property#

The selected timer can be started by a Frame Burst Active signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.FrameBurstTriggerWait Property#

The selected timer can be started by a Frame Burst Trigger Wait signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.FrameTriggerWait Property#

The selected timer can be started by a Frame Trigger Wait signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Line1 Property#

The selected timer can be started by a Line 1 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Line2 Property#

The selected timer can be started by a Line 2 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Line3 Property#

The selected timer can be started by a Line 3 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Line4 Property#

The selected timer can be started by a Line 4 signal.

Applies to: dart 2 USB and dart USB

PLCamera.TimerTriggerSourceEnum.Name Property#

The full name of TimerTriggerSource

PLCamera.TimerTriggerSourceEnum.Off Property#

The selected timer is disabled and can't be started.

Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.PeriodicSignal1 Property#

The selected timer can be started by a Periodic Signal 1 signal.

Applies to: ace 2 GigE

PLCamera.TimerTriggerSourceEnum.SoftwareSignal1 Property#

The selected timer can be started by a Software Signal 1 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.SoftwareSignal2 Property#

The selected timer can be started by a Software Signal 2 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.SoftwareSignal3 Property#

The selected timer can be started by a Software Signal 3 signal.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Timer1Active Property#

The selected timer can be started by a Timer 1 Active signal. By default, a Timer 1 Active signal is generated whenever timer 1 has been started. You can change this behavior using the Counter Event Activation parameter.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Timer1End Property#

The selected timer can be started by a Timer 1 End signal. A Timer 1 End signal is generated whenever timer 1 has elapsed.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Timer2Active Property#

The selected timer can be started by a Timer 2 Active signal. By default, a Timer 2 Active signal is generated whenever timer 2 is started. You can change this behavior using the Counter Event Activation parameter.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP

PLCamera.TimerTriggerSourceEnum.Timer2End Property#

The selected timer can be started by a Timer 2 End signal. A Timer 2 End signal is generated whenever timer 2 has elapsed.

Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, boost CoaXPress, dart 2 USB, dart USB and racer 2 CXP