Transport Layer#
Namespaces#
Name |
---|
Pylon::Key This namespace contains keys for accessing the properties of pylon info objects. |
Classes#
Name | |
---|---|
class | Pylon::DeviceInfoList STL std::vector like container for Pylon::CDeviceInfo objects. |
class | Pylon::TlInfoList STL std::vector like container for Pylon::CTlInfo objects. |
class | Pylon::AccessModeSet Collection of access mode bits. |
class | Pylon::CDeviceInfo Holds information about an enumerated device. |
class | Pylon::CTlFactory the Transport Layer Factory |
class | Pylon::CTlInfo Class used for storing the result of the transport layer enumeration process. |
struct | Pylon::GigEActionCommandResult Optional result structure of IGigETransportLayer::IssueActionCommand and IGigETransportLayer::IssueScheduledActionCommand. |
interface | Pylon::IDeviceFactory Interface to be implemented by device factories used to create devices. |
interface | Pylon::IInterface An interface is used to represent a frame grabber board, a network card, etc. |
interface | Pylon::ITransportLayer The interface of Transport Layer objects. |
interface | Pylon::IGigETransportLayer Extends the ITransportLayer interface by GigE Vision specific functionality. |
Types#
Name | |
---|---|
enum | EDeviceAccessMode { Control = 0x1, Stream = 0x3, Event = 0x4, Exclusive = 0x5, _NumModes} The available access modes when opening a camera object. |
enum | EDeviceAccessiblityInfo { Accessibility_Unknown = 0, Accessibility_Ok = 1, Accessibility_Opened = 2, Accessibility_OpenedExclusively = 3, Accessibility_NotReachable = 4} Information about the accessibility of a device. |
enum | EGigEActionCommandStatus { GigEActionCommandStatus_Ok = 0, GigEActionCommandStatus_NoRefTime = 0xE1018013, GigEActionCommandStatus_Overflow = 0xE1018015, GigEActionCommandStatus_ActionLate = 0xE1018016} Lists possible status codes returned by IGigETransportLayer::IssueActionCommand or IGigETransportLayer::IssueScheduledActionCommand. |
Functions#
Name | |
---|---|
AccessModeSet & | set(size_t pos) Sets the bit at position pos. |
AccessModeSet & | reset() Resets all bits to zero. |
bool | any() const Returns whether any of the bits is set (i.e., whether at least one bit in the AccessModeSet is set to one). |
bool | none() const Returns whether any of the bits is set (i.e., whether at least one bit in the AccessModeSet is set to one). |
bool | test(size_t pos) const Returns whether the bit at position pos is set (i.e., whether it is one). |
unsigned long | to_ulong() const Returns an unsigned long with the integer value that has the same bits set as the AccessModeSet. |
AccessModeSet | operator+(EDeviceAccessMode lhs, EDeviceAccessMode rhs) Creates a set containing lhs and rhs operands. |
AccessModeSet | **[operator |
AccessModeSet | operator+(const AccessModeSet & lhs, EDeviceAccessMode rhs) Adds the operand rhs to the set lhs. |
AccessModeSet | **[operator |
bool | operator==(const AccessModeSet & lhs, const AccessModeSet & rhs) Check if the operand rhs is equal to lhs. |
bool | operator!=(const AccessModeSet & lhs, const AccessModeSet & rhs) Check if the operand rhs is not equal to lhs. |
std::ostream & | operator<<(std::ostream & ostr, const Pylon::AccessModeSet & ams) |
Attributes#
Name | |
---|---|
const char *const | BaslerGigEDeviceClass This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory. |
const char *const | BaslerCamEmuDeviceClass This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory. |
const char *const | BaslerIpCamDeviceClass This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory. |
const char *const | BaslerCameraLinkDeviceClass This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory. |
const char *const | BaslerGenTlDeviceClassPrefix The actual device class string is made up of this prefix + '/' + [TL Vendor] + '/' + [TL Model]. |
const char *const | BaslerGenTlCxpDeviceClass This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory. |
const char *const | BaslerGenTlBlazeDeviceClass This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory. |
const char *const | BaslerUsbDeviceClass This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory. |
Detailed Description#
The Transport Layer Factory or a Transport Layer object are used to enumerate and create pylon Devices.
An Instant Camera uses a pylon Device internally for operation. The term 'transport layer' is used as an abstraction for a physical interface such as USB, GigE, or Camera Link. You can find more information here:
- [Transport Layers]
- [Transport Layer Factory]
- [Creating a pylon Device]
- [Enumerating and Creating pylon Devices]
Types Documentation#
enum EDeviceAccessMode#
Enumerator | Value | Description |
---|---|---|
Control | 0x1 | access the control and status registers |
Stream | 0x3 | access a streaming data channel |
Event | 0x4 | access the event data channel |
Exclusive | 0x5 | exclusive access to the device |
_NumModes |
The available access modes when opening a camera object.
enum EDeviceAccessiblityInfo#
Enumerator | Value | Description |
---|---|---|
Accessibility_Unknown | 0 | The accessibility could not be determined. The state of accessibility is unknown. |
Accessibility_Ok | 1 | The device could be opened. |
Accessibility_Opened | 2 | The device is reachable, but can be opened in read only mode only. |
Accessibility_OpenedExclusively | 3 | The device is reachable, but currently opened exclusively by another application. |
Accessibility_NotReachable | 4 | The device could not be reached or does not exist. No connection to the device is possible. |
Information about the accessibility of a device.
enum EGigEActionCommandStatus#
Enumerator | Value | Description |
---|---|---|
GigEActionCommandStatus_Ok | 0 | The device acknowledged the command. |
GigEActionCommandStatus_NoRefTime | 0xE1018013 | The device is not synchronized to a master clock to be used as time reference. Typically used when scheduled action commands cannot be scheduled for a future time since the reference time coming from IEEE 1588 is not locked. The action command has been ignored by the device. |
GigEActionCommandStatus_Overflow | 0xE1018015 | Returned when the scheduled action commands queue is full and the device cannot accept the additional request. The action command has been discarded by the device. |
GigEActionCommandStatus_ActionLate | 0xE1018016 | The requested scheduled action command was requested at a point in time that is in the past. If the time tag of the scheduled action command is in the past (relative to the device timestamp), and if it is a valid action command, then the device will execute this action command immediately and return GigEActionCommandStatus_ActionLate . This status code is used as an indicator to the application requesting the action command that a mis-synchronization might have occurred. |
Lists possible status codes returned by IGigETransportLayer::IssueActionCommand or IGigETransportLayer::IssueScheduledActionCommand.
Functions Documentation#
function set#
Sets the bit at position pos.
Parameters:
- pos Order position of the bit whose value is modified. Order positions are counted from the rightmost bit, which is order position 0.
Return: *this
function reset#
Resets all bits to zero.
Return: *this
function any#
Returns whether any of the bits is set (i.e., whether at least one bit in the AccessModeSet is set to one).
Return: true if any of the bits in the AccessModeSet is set (to one), and false otherwise.
function none#
Returns whether any of the bits is set (i.e., whether at least one bit in the AccessModeSet is set to one).
Return: true if any of the bits in the AccessModeSet is set (to one), and false otherwise.
function test#
Returns whether the bit at position pos is set (i.e., whether it is one).
Parameters:
- pos Order position of the bit whose value is modified. Order positions are counted from the rightmost bit, which is order position 0.
Return: true if the bit at position pos is set, and false if it is not set.
function to_ulong#
Returns an unsigned long with the integer value that has the same bits set as the AccessModeSet.
Return: Integer value with the same bit representation as the AccessModeSet object.
function operator+#
Creates a set containing lhs and rhs operands.
Parameters:
- lhs left operand
- rhs right operand
Return: returns an AccessModeSet containing both operands
function operator|#
Creates a set containing lhs and rhs operands.
Parameters:
- lhs left operand
- rhs right operand
function operator+#
Adds the operand rhs to the set lhs.
Parameters:
- lhs a set of bits.
- rhs the additional bit
function operator|#
Adds the operand rhs to the set lhs.
Parameters:
- lhs a set of bits.
- rhs the additional bit
function operator==#
Check if the operand rhs is equal to lhs.
Parameters:
- lhs a set of bits.
- rhs the additional set of bits.
function operator!=#
Check if the operand rhs is not equal to lhs.
Parameters:
- lhs a set of bits.
- rhs the additional set of bits.
function operator<<#
STL operator out
Attributes Documentation#
variable BaslerGigEDeviceClass#
This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory.
variable BaslerCamEmuDeviceClass#
This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory.
variable BaslerIpCamDeviceClass#
This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory.
variable BaslerCameraLinkDeviceClass#
This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory.
variable BaslerGenTlDeviceClassPrefix#
The actual device class string is made up of this prefix + '/' + [TL Vendor] + '/' + [TL Model].
variable BaslerGenTlCxpDeviceClass#
This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory.
variable BaslerGenTlBlazeDeviceClass#
const char *const BaslerGenTlBlazeDeviceClass = "BaslerGTC/Basler/GenTL_Producer_for_Basler_blaze_101_cameras";
This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory.
variable BaslerUsbDeviceClass#
This device class can be used to create the corresponding Transport Layer object or when creating Devices with the Transport Layer Factory.