PLCamera.UserDefinedValueSelectorEnum Class#
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB
Visibility: Guru
Selecting Parameters: UserDefinedValue
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.UserDefinedValueSelectorEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.UserDefinedValueSelectorEnum | Initializes a new instance of the PLCamera.UserDefinedValueSelectorEnum class |
Properties#
Name | Description | |
---|---|---|
Name | The full name of UserDefinedValueSelector (Overrides ParameterListEnum.Name.) | |
Value1 | The user-defined value 1 can be configured. Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB | |
Value2 | The user-defined value 2 can be configured. Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB | |
Value3 | The user-defined value 3 can be configured. Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB | |
Value4 | The user-defined value 4 can be configured. Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB | |
Value5 | The user-defined value 5 can be configured. Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB |
Methods#
Name | Description | |
---|---|---|
ToString | The full name of UserDefinedValueSelector (Overrides Object.ToString()()()().) |
PLCamera.UserDefinedValueSelectorEnum.ToString Method#
The full name of UserDefinedValueSelector
Return Value#
Type: String
Returns the full name of UserDefinedValueSelector
PLCamera.UserDefinedValueSelectorEnum Constructor#
Initializes a new instance of the PLCamera.UserDefinedValueSelectorEnum class
PLCamera.UserDefinedValueSelectorEnum.Name Property#
The full name of UserDefinedValueSelector
PLCamera.UserDefinedValueSelectorEnum.Value1 Property#
The user-defined value 1 can be configured.
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB
PLCamera.UserDefinedValueSelectorEnum.Value2 Property#
The user-defined value 2 can be configured.
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB
PLCamera.UserDefinedValueSelectorEnum.Value3 Property#
The user-defined value 3 can be configured.
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB
PLCamera.UserDefinedValueSelectorEnum.Value4 Property#
The user-defined value 4 can be configured.
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB
PLCamera.UserDefinedValueSelectorEnum.Value5 Property#
The user-defined value 5 can be configured.
Applies to: CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB