PLCamera.ExposureTimeModeEnum Class#
Applies to: GigE and ace USB
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ExposureTimeModeEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.ExposureTimeModeEnum | Initializes a new instance of the PLCamera.ExposureTimeModeEnum class |
Properties#
Name | Description | |
---|---|---|
Name | The full name of ExposureTimeMode (Overrides ParameterListEnum.Name.) | |
Standard | The exposure time mode is set to Standard. Applies to: GigE and ace USB | |
UltraShort | The exposure time mode is set to Ultra Short. Applies to: GigE and ace USB |
Methods#
Name | Description | |
---|---|---|
ToString | The full name of ExposureTimeMode (Overrides Object.ToString()()()().) |
PLCamera.ExposureTimeModeEnum.ToString Method#
The full name of ExposureTimeMode
Return Value#
Type: String
Returns the full name of ExposureTimeMode
PLCamera.ExposureTimeModeEnum Constructor#
Initializes a new instance of the PLCamera.ExposureTimeModeEnum class
PLCamera.ExposureTimeModeEnum.Name Property#
The full name of ExposureTimeMode
PLCamera.ExposureTimeModeEnum.Standard Property#
The exposure time mode is set to Standard.
Applies to: GigE and ace USB
PLCamera.ExposureTimeModeEnum.UltraShort Property#
The exposure time mode is set to Ultra Short.
Applies to: GigE and ace USB