PLCamera.AcquisitionModeEnum Class#
Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP
Visibility: Beginner
Selecting Parameters: AcquisitionAbort, AcquisitionStart, AcquisitionStop
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.AcquisitionModeEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.AcquisitionModeEnum | Initializes a new instance of the PLCamera.AcquisitionModeEnum class |
Properties#
Name | Description | |
---|---|---|
Continuous | The acquisition mode is set to Continuous. The camera will acquire images until acquisition is stopped. Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP | |
MultiFrame | The acquisition mode is set to Multi Frame. The camera will acquire a number of images specified by the user. Applies to: CameraLink and GigE | |
Name | The full name of AcquisitionMode (Overrides ParameterListEnum.Name.) | |
SingleFrame | The acquisition mode is set to Single Frame. The camera will acquire a single image. Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP |
Methods#
Name | Description | |
---|---|---|
ToString | The full name of AcquisitionMode (Overrides Object.ToString()()()().) |
PLCamera.AcquisitionModeEnum.ToString Method#
The full name of AcquisitionMode
Return Value#
Type: String
Returns the full name of AcquisitionMode
PLCamera.AcquisitionModeEnum Constructor#
Initializes a new instance of the PLCamera.AcquisitionModeEnum class
PLCamera.AcquisitionModeEnum.Continuous Property#
The acquisition mode is set to Continuous. The camera will acquire images until acquisition is stopped.
Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP
PLCamera.AcquisitionModeEnum.MultiFrame Property#
The acquisition mode is set to Multi Frame. The camera will acquire a number of images specified by the user.
Applies to: CameraLink and GigE
PLCamera.AcquisitionModeEnum.Name Property#
The full name of AcquisitionMode
PLCamera.AcquisitionModeEnum.SingleFrame Property#
The acquisition mode is set to Single Frame. The camera will acquire a single image.
Applies to: CamEmu, CameraLink, GigE, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP