Basler Vision Connector Messaging: Starting Image Streaming
With the Basler Vision Connector you can control the image streaming by starting and stopping the image stream. The control doesn't affect any camera property, including the trigger definitions. If you want to change these camera properties, see the messages described in Setting Camera Quick Parameters.
With the following command you can initiate image streaming for a specific camera. When you activate it, continuous streaming publishes images to the streaming topic. For triggered image acquisition, the Basler Vision Connector sends images based on trigger configurations defined via the camera parameters.
JSON Payload
Field | Optional | Type | Description |
TransactionID | Yes | String | Transaction identification |
Action | No | String | Method called. Fixed value: StartStreaming |
DeviceID | No | String | Device identification |
FrameCount | Yes | Integer | Number of frames to be streamed. Values less than 1 are invalid. If no frame count is provided, the camera streams continuously until you stop the streaming. |
{
"TransactionID": "12341263412635465",
"Action": "StartStreaming",
"DeviceID": "548451887",
"FrameCount": 100
}
Response Object
Field | Optional | Type | Description |
TransactionID | Yes | String | Transaction identification |
ReturnCode | No | Integer (32-bit unsigned) | Message code following Message Codes |
Message | Yes | String | Response message |
{
"TransactionID": "12341263412635465",
"ReturnCode": 0,
"Message": "Stream started."
}